This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BlackHawk USB560v2 system trace仿真器



我的仿真器也是这个问题,usb灯是红色,模式的灯绿色闪烁。怎么解决的呀?

  • 请问您现在使用的CCS版本以及芯片型号是什么?

    电脑的设备管理器中能否识别仿真器?若是可以的话,连接CCS测试,具体的错误提示是什么?

    另外请先参考下面的讨论贴

    www.blackhawk-dsp.com/.../usb560v2

    e2e.ti.com/.../831082

    e2e.ti.com/.../732161
  • yang 您好,设备管理器不识别仿真器,换了5个电脑都不识别。usb灯红色,模式灯绿色闪烁。
  • 是否有重新安装驱动?请先尝试安装一下驱动,一般在CCS的安装文件夹内

    C:\ti\ccs1000\ccs\ccs_base\emulation\Blackhawk
  • 重新装过驱动,还是不行,usb红灯是不是usb硬件出现问题了?
  • [Start: Blackhawk XDS560v2-USB System Trace Emulator_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\IPITRT\AppData\Local\TEXASI~1\CCS\
    ccs1000\0\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560/2xx-class product.
    This utility will load the program 'bh560v2u.out'.
    E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
    Download failed for file D:\ti\ccs1000\ccs\ccs_base\common\uscif\xds560v2.out

    An error occurred while soft opening the controller.

    -----[An error has occurred and this utility has aborted]--------------------

    This error is generated by TI's USCIF driver or utilities.

    The value is '-250' (0xffffff06).
    The title is 'SC_ERR_ECOM_EMUNAME'.

    The explanation is:
    An attempt to access the debug probe via USCIF ECOM has failed.

    [End: Blackhawk XDS560v2-USB System Trace Emulator_0]