This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何用28377的ecap功能实现连续采样PWM波的频率

Other Parts Discussed in Thread: C2000WARE

我想用28377的ecap功能来实现连续采样PWM波的频率,ecap时钟用系统时钟200M,连续采样周期值先放在ecap1的寄存器CAP1-4中。再利用epwm的计数功能,每1/40kHz个周期触发中断,在中断程序里将CAP1-4的数值取出计算频率。下面是我的ecap部分的程序,但是一直采样不到频率,寄存器CAP1-4的值也没有。

//主程序里的ECAP设置 

  void InitECapture();
    GPIO_SetupPinOptions(19,GPIO_INPUT,GPIO_ASYNC); 
    void SetCap1Mode();

void InitECapture(void)
  {
    EALLOW;
    InputXbarRegs.INPUT7SELECT = 19;       // Set eCAP1 source to GPIO-pin
    EDIS;
    //GpioCtrlRegs.GPAPUD.bit.GPIO24=0;
    //GpioCtrlRegs.GPAQSEL2.bit.GPIO24=0;
    //GpioCtrlRegs.GPAMUX2.bit.GPIO24=1;
    //EDIS;
  }
void SetCap1Mode(void)
  {
     ECap1Regs.ECEINT.all = 0x0000;             // Disable all capture __interrupts
     ECap1Regs.ECCLR.all = 0xFFFF;              // Clear all CAP __interrupt flags
     ECap1Regs.ECCTL1.bit.CAPLDEN = 0;          // Disable CAP1-CAP4 register loads
     ECap1Regs.ECCTL2.bit.TSCTRSTOP = 0;        // Make sure the counter is stopped

     ECap1Regs.ECCTL1.bit.CAP1POL=0;  //捕捉上升沿
     ECap1Regs.ECCTL1.bit.CAP2POL=0;
     ECap1Regs.ECCTL1.bit.CAP3POL=0;
     ECap1Regs.ECCTL1.bit.CAP4POL=0;
     ECap1Regs.ECCTL1.bit.CTRRST1=1;  //差分模式
     ECap1Regs.ECCTL1.bit.CTRRST2=1;
     ECap1Regs.ECCTL1.bit.CTRRST3=1;
     ECap1Regs.ECCTL1.bit.CTRRST4=1;
     ECap1Regs.ECCTL1.bit.CAPLDEN=1;  //使能事件捕捉时捕捉寄存器装载计算器值
     ECap1Regs.ECCTL1.bit.PRESCALE=00000; //不分频
     ECap1Regs.ECCTL2.bit.CAP_APWM=0; //捕捉模式
     ECap1Regs.ECCTL2.bit.CONT_ONESHT=0;  //连续模式
     ECap1Regs.ECCTL2.bit.SYNCO_SEL=2;  //屏蔽0x0010
     ECap1Regs.ECCTL2.bit.SYNCI_EN=0;  //屏蔽
     ECap1Regs.ECEINT.all=0x0000;   //关闭所有CAP中断
     ECap1Regs.ECCLR.all=0xFFFF;    //清除所有中断标志
     ECap1Regs.ECCTL2.bit.TSCTRSTOP=1; //启动计数
     //eCAP1Regs.ECEINT.bit.CEVT4=1;   //使能4级事件中断

  }

//中断程序采样频率取值
    T1=ECap1Regs.CAP1;
    T2=ECap1Regs.CAP2;
    T3=ECap1Regs.CAP3;
    T4=ECap1Regs.CAP4;
    fs=200000*1000*(1/T1+1/T2+1/T3+1/T4)/4;

  • 你好,官方提供了两个eCAP捕获ePWM的例程是否有参考过?有没有确认过GPIO口是否设置正确?
  • C:\ti\c2000\C2000Ware_3_02_00_00\device_support\f2837xd\examples\cpu1\ecap_capture_pwm
    C:\ti\c2000\C2000Ware_3_02_00_00\device_support\f2837xd\examples\cpu1\ecap_capture_pwm_xbar
  • 感谢您的回复,我再参考了下例程,这两个都是单次捕获模式的,同时设置上我也参考了下,应该是没问题。

    GPIO口的设置不是这个函数吗

    //Setup up the GPIO input/output options for the specified pin.
    //The flags are a 16-bit mask produced by ORing together options.
    //For input pins, the valid flags are:
    //GPIO_PULLUP    Enable pull-up
    //GPIO_INVERT    Enable input polarity inversion
    //GPIO_SYNC        Synchronize the input latch to PLLSYSCLK (default -- you don't need to specify this)
    //GPIO_QUAL3    Use 3-sample qualification
    //GPIO_QUAL6    Use 6-sample qualification
    //GPIO_ASYNC    Do not use synchronization or qualification
    //(Note: only one of SYNC, QUAL3, QUAL6, or ASYNC is allowed)
    //
    //For output pins, the valid flags are:
    //GPIO_OPENDRAIN    Output in open drain mode
    //GPIO_PULLUP        If open drain enabled, also enable the pull-up
    //and the input qualification flags (SYNC/QUAL3/QUAL6/SYNC) listed above.
    //
    //With no flags, the default input state is synchronous with no
    //pull-up or polarity inversion. The default output state is
    //the standard digital output.
    void GPIO_SetupPinOptions(Uint16 pin, Uint16 output, Uint16 flags)
    {
        volatile Uint32 *gpioBaseAddr;
        volatile Uint32 *dir, *pud, *inv, *odr, *qsel;
        Uint32 pin32, pin16, pinMask, qual;

        pin32 = pin % 32;
        pin16 = pin % 16;
        pinMask = 1UL << pin32;
        gpioBaseAddr = (Uint32 *)&GpioCtrlRegs + (pin/32)*GPY_CTRL_OFFSET;

        //Create pointers to the appropriate registers. This is a workaround
        //for the way GPIO registers are defined. The standard definition
        //in the header file makes it very easy to do named accesses of one
        //register or bit, but hard to do arbitrary numerical accesses. It's
        //easier to have an array of GPIO modules with identical registers,
        //including arrays for multi-register groups like GPyQSEL1-2. But
        //the header file doesn't define anything we can turn into an array,
        //so manual pointer arithmetic is used instead.
        dir = gpioBaseAddr + GPYDIR;
        pud = gpioBaseAddr + GPYPUD;
        inv = gpioBaseAddr + GPYINV;
        odr = gpioBaseAddr + GPYODR;
        qsel = gpioBaseAddr + GPYQSEL + pin32/16;

        EALLOW;

        //Set the data direction
        *dir &= ~pinMask;
        if (output == 1)
        {
            //Output, with optional open drain mode and pull-up
            *dir |= pinMask;

            //Enable open drain if necessary
            if (flags & GPIO_OPENDRAIN)
                *odr |= pinMask;
            else
                *odr &= ~pinMask;

            //Enable pull-up if necessary. Open drain mode must be active.
            if (flags & (GPIO_OPENDRAIN | GPIO_PULLUP))
                *pud &= ~pinMask;
            else
                *pud |= pinMask;
        } else
        {
            //Input, with optional pull-up, qualification, and polarity inversion
            *dir &= ~pinMask;

            //Enable pull-up if necessary
            if (flags & GPIO_PULLUP)
                *pud &= ~pinMask;
            else
                *pud |= pinMask;

            //Invert polarity if necessary
            if (flags & GPIO_INVERT)
                *inv |= pinMask;
            else
                *inv &= ~pinMask;
        }

        //Extract the qualification parameter and load it into the register. This is
        //also needed for open drain outputs, so we might as well do it all the time.
        qual = (flags & GPIO_ASYNC) / GPIO_QUAL3;
        *qsel &= ~(0x3L << (2 * pin16));
        if (qual != 0x0)
            *qsel |= qual << (2 * pin16);

        EDIS;
    }