This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI原厂Spectrum Digital仿真器XDS560v2STM电脑无法发现驱动



电脑都发现不了驱动,错误log:

[Start: Blackhawk XDS560v2-USB System Trace Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\uidq1196\AppData\Local\TEXASI~1\
CCS\ccs1000\2\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
E_RPCENV_IO_ERROR(-6) No connection: emulator was not found
Download failed for file D:\software\ti\ccs1000\ccs\ccs_base\common\uscif\xds560v2.out

An error occurred while soft opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.

The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.

[End: Blackhawk XDS560v2-USB System Trace Emulator_0]