设计了一个28335板子,错把XRD引脚当作普通IO口用了(我以为所有的引脚都可以复用)。
我的问题如下:
1)在不实用XINTF时,可以直接让XRD输出低电平或高电平吗?
2)如果1)的问题为否定的,那么可以让XRD引脚和旁边的GPIO37(PIN150)短接起来吗?这样可以通过GPIO37来实现IO功能,但这样会不会相当于把XRD引脚短路进而使得芯片损坏?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设计了一个28335板子,错把XRD引脚当作普通IO口用了(我以为所有的引脚都可以复用)。
我的问题如下:
1)在不实用XINTF时,可以直接让XRD输出低电平或高电平吗?
2)如果1)的问题为否定的,那么可以让XRD引脚和旁边的GPIO37(PIN150)短接起来吗?这样可以通过GPIO37来实现IO功能,但这样会不会相当于把XRD引脚短路进而使得芯片损坏?
这个引脚本身就是低电平的?This signal is driven low on all bus modes and data size types.
user1569241 说:让XRD引脚和旁边的GPIO37(PIN150)短接起来吗?这样可以通过GPIO37来实现IO功能
没明白这样做的目的是什么?GPIO37单独配置为IO口就可以了,为什么要短接起来再实现IO功能?