首次正常烧入程序,再次烧入程序时出现这个问题,后续一直能够复现。首次烧入的程序一直能够正常工作,证明DSP芯片正常,仿真器也是正常工作。求大神解答!
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Flash Programmer: Warning: The configured device (TMS320F28377S), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc12b: (Error -1066 @ 0xC12B) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 6.0.628.1)
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint
C28xx_CPU1: Error writing the PLL values. (Flash algorithm returned error code). Operation cancelled.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File: D:\workspace_v6_2\Thermostat_48\Debug\Thermostat_48.out: Load failed.
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc0af: (Error -1066 @ 0xC0AF) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 6.0.628.1)
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint
C28xx_CPU1: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc0af: (Error -1066 @ 0xC0AF) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 6.0.628.1)
C28xx_CPU1: Breakpoint Manager: Retrying with a AET breakpoint