XINTF配置如下
void InitXintf(void) {
// This shows how to write to the XINTF registers. The
// values used here are the default state after reset.
// Different hardware will require a different configuration.
// For an example of an XINTF configuration used with the
// F28335 eZdsp, refer to the examples/run_from_xintf project.
// Any changes to XINTF timing should only be made by code
// running outside of the XINTF.
// All Zones---------------------------------
// Timing for all zones based on XTIMCLK = 1/2 SYSCLKOUT
EALLOW;
SysCtrlRegs.PCLKCR3.bit.XINTFENCLK = 1;
EDIS;
EALLOW;
XintfRegs.XINTCNF2.bit.XTIMCLK = 1;
// No write buffering
XintfRegs.XINTCNF2.bit.WRBUFF = 0;
// XCLKOUT is enabled
XintfRegs.XINTCNF2.bit.CLKOFF = 0;
// XCLKOUT = XTIMCLK/2
XintfRegs.XINTCNF2.bit.CLKMODE = 1;
// Zone 0------------------------------------
// When using ready, ACTIVE must be 1 or greater
// Lead must always be 1 or greater
// Zone write timing
XintfRegs.XTIMING0.bit.XWRLEAD = 3;
XintfRegs.XTIMING0.bit.XWRACTIVE = 7;
XintfRegs.XTIMING0.bit.XWRTRAIL = 3;
// Zone read timing
XintfRegs.XTIMING0.bit.XRDLEAD = 3;
XintfRegs.XTIMING0.bit.XRDACTIVE = 7;
XintfRegs.XTIMING0.bit.XRDTRAIL = 3;
// double all Zone read/write lead/active/trail timing
XintfRegs.XTIMING0.bit.X2TIMING = 1;
// Zone will sample XREADY signal
XintfRegs.XTIMING0.bit.USEREADY = 1; //修改值,忽略xready信号
XintfRegs.XTIMING0.bit.READYMODE = 1; // sample asynchronous
// Size must be either:
// 0,1 = x32 or
// 1,1 = x16 other values are reserved
XintfRegs.XTIMING0.bit.XSIZE = 3;
EDIS;
}
使用ZONE0区域 通信代码如下
void CommunicationFPGA(void)
{
GpioDataRegs.GPACLEAR.bit.GPIO5 = 1; //D_G_A 使能A相数据总线收发器
GpioDataRegs.GPASET.bit.GPIO30 = 1; //D_G_B 禁止B相总线收发器导通
GpioDataRegs.GPBSET.bit.GPIO32 = 1; //D_G_C 禁止C相总线收发器导通
GpioDataRegs.GPACLEAR.bit.GPIO2 = 1; //A_G_A****地址线总线收发器使能,低电平使能
GpioDataRegs.GPASET.bit.GPIO1 = 1; //A_G_B地址总线禁止
GpioDataRegs.GPBSET.bit.GPIO39 = 1; //A_G_C
GpioDataRegs.GPASET.bit.GPIO4 = 1; //D_DIR_A 总线收发器方向,DSP->FPGA
GpioDataRegs.GPASET.bit.GPIO3 = 1;
*(sendStart + 0) =Value;
*(sendStart + 1) =Value;
*(sendStart + 2) =Value;
*(sendStart + 3) =Value;
*(sendStart + 4) =Value;
*(sendStart + 5) =Value;
*(sendStart + 6) =Value;
*(sendStart + 7) =Value;
GpioDataRegs.GPACLEAR.bit.GPIO4 = 1; //D_DIR_A 总线收发器方向,FPAG->DSP
GpioDataRegs.GPASET.bit.GPIO3 = 1;
/* receFPGAmessage[0] = *(receStart + 0); //第一个子模块电压
receFPGAmessage[1] = *(receStart + 1); //第二个子模块电压
receFPGAmessage[2] = *(receStart + 2); //第三个子模块电压
receFPGAmessage[3] = *(receStart + 3); //第三个子模块电压
receFPGAmessage[4] = *(receStart + 4); //第四个子模块电压
receFPGAmessage[5] = *(receStart + 5);
receFPGAmessage[6] = *(receStart + 6);
receFPGAmessage[7] = *(receStart + 7); //第六个子模块电压
receFPGAmessage[8] = *(receStart + 8); //第七个子模块电压
receFPGAmessage[9] = *(receStart + 9); //第七个子模块电压
receFPGAmessage[10] = *(receStart + 10); //第八个子模块电压
receFPGAmessage[11] = *(receStart + 11); //第八个子模块电压
receFPGAmessage[12] = *(receStart + 12); //第八个子模块电压
receFPGAmessage[13] = *(receStart + 13); //第八个子模块电压
receFPGAmessage[14] = *(receStart + 14); //第八个子模块电压
receFPGAmessage[15] = *(receStart + 15); //第八个子模块电压*/
GpioDataRegs.GPASET.bit.GPIO5 = 1; //D_G_A 禁止A相数据总线收发器
GpioDataRegs.GPASET.bit.GPIO2 = 1; //A_G_A禁止A相地址总线收发
return;
}
Value值为9;
仿真时,通过查看memory观察,数据异常,而且没有什么规律
已经测试过FPGA时序是正常的
求大神告知