This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

这是什么错误



This project was created using a version of compiler that is not currently installed - 6.1.0 [C2000]. Another version of the compiler will be used during build - 18.12.2.LTS. See 'Help > Install New Software' and select 'Code Generation Tools Updates' to check if this compiler is available through a CCS update. Visit <a href="liveaction:OpenAppCenter">CCS App Center</a> to get the latest compiler support. Or <a href="software-dl.ti.com/.../a> and install the compiler, then register it with CCS through 'Preferences > CCS > Build > Compilers'.

  • This project was created using a version of compiler that is not currently installed - 6.1.0 [C2000].

    根据提示,您现在没有该工程创建时使用的6.1.0版本的compiler,所以会使用您现在已经安装的其他版本的compiler。

    您可以根据提示来安装6.1.0版本的compiler或者没有错误的话也无需安装