This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F280049程序下载问题



我把以前F280049 64PIN的代码,用来下载到F280049 100PIN的芯片里,出现芯片掉电后,程序就不存在了,应该是没有下载进Flash里面,请问,这是什么原因导致的呢?

  • RAM运行还是FLASH运行?在TI例程代码中有这样的语句,您看一下您的代码内是否有这样的语句? 

    //*****************************************************************************
    //*****************************************************************************
    //
    //! \internal
    //! Checks that a pin number is valid for a device.
    //!
    //! Note that this function reflects the highest possible GPIO number of a
    //! device on its biggest package. Check the datasheet to see what the actual
    //! range of valid pin numbers is for a specific package.
    //!
    //! \return None.
    //
    //*****************************************************************************
    #ifdef DEBUG
    static inline bool
    GPIO_isPinValid(uint32_t pin)
    {
        return((pin <= 59U) || ((pin >= 224U) && (pin <= 247U)));
    }
    #endif

  • 经过试验发现是GPIO24与GPIO32没有上拉导致,这两个GPIO内部难道没有自动上拉吗?
  • 参考数据手册 4.5 Pins With Internal Pullup and Pulldown

    默认都是Pullup disabled的

    上拉电阻的使用主要取决于该引脚的应用程序。您是否正在使用此引导模式引脚?

    在F280049 controlCARD中,GPIO24和GPIO32都已通过56K电阻上拉。