This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[分享]F2837x GPIO使用DAT問題



假設 GpioDataRegs.GPADAT.all的值為0x0000

此時設定GPIO1與GPIO2為1

GpioDataRegs.GPADAT.bit.GPIO1 = 1; 

GpioDataRegs.GPADAT.bit.GPIO2 = 1;

當設定GPIO2的時候會將  GpioDataRegs.GPADAT.all讀出(此時GPIO1為0),再將GPIO的bit設置為1再存入GpioDataRegs.GPADAT.all。

將導致GPIO1為0,手冊上的解決方法為

1.GPIO1與GPIO2之間增加延遲

2.使用GPASET

使用手冊:

GpioDataRegs.GPADAT.bit.GPIO1 = 1; //I1 performs read-modify-
write of GPADAT GpioDataRegs.GPADAT.bit.GPIO2 = 1; //I2 also a read-modify-
write of GPADAT. //GPADAT gets the old value of GPIO1 due to the delay
The second instruction will wait for the first to finish its write due to the write-followed-by-read
protection on this peripheral frame. There will be some lag, however, between the write of (I1) and the
GPyDAT bit reflecting the new value (1) on the pin. During this lag, the second instruction will read the
old value of GPIO1 (0) and write it back along with the new value of GPIO2 (1). Therefore, GPIO1 pin
stays low.
One solution is to put some NOPs between instructions. A better solution is to use the
GPySET/GPyCLEAR/GPyTOGGLE registers instead of the GPyDAT registers. These registers always
read back a 0 and writes of 0 have no effect. Only bits that need to be changed can be specified
without disturbing any other bit(s) that are currently in the process of changing.