This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2808的SCIB無法進入中斷



各位大神好,使用範例程式如下:

GPIO 設定為GPIO28&GPIO29作為SCI通訊

但無法進入中斷

debug模式無法接收資料

// TI File $Revision: /main/7 $

// Checkin $Date: June 13, 2007   10:28:33 $

//###########################################################################

//

// FILE: Example_280xSci_Autobaud_.c

//

// TITLE: DSP280x SCI Autobaud detect example

//

// ASSUMPTIONS:

//

//    This program requires the DSP280x header files.

//

//    Test requires the following hardware connections:

//

//          GPIO29/SCITXDA <-> GPIO19/SCIRXDB

//          GPIO28/SCIRXDA <-> GPIO18/SCITXDB

//

//

//    As supplied, this project is configured for "boot to SARAM"

//    operation.  The 280x Boot Mode table is shown below.

//    For information on configuring the boot mode of an eZdsp,

//    please refer to the documentation included with the eZdsp,

//

//       Boot      GPIO18     GPIO29    GPIO34

//       Mode      ***    SCITXDA

//                  SCITXB

//       -------------------------------------

//       Flash       1          1        1

//       SCI-A       1          1        0

//       SPI-A       1          0        1

//       I2C-A       1          0        0

//       ECAN-A      0          1        1

//       SARAM       0          1        0  <- "boot to SARAM"

//       OTP         0          0        1

//       I/0         0          0        0 //

//

//    This test will perform autobaud lock at a variety of baud rates, including

//    very high baud rates.

//

//    For this test to properly run, connect the SCI-A pins to the

//    SCI-B pins without going through a transciever.

//

//    At higher baud rates, the slew rate of the incoming data bits can be

//    affected by transceiver and connector performance. This slew rate may

//    limit reliable autobaud detection at higher baud rates.

//

//    SCIA: Slave, autobaud locks, receives characters and

//          echos them back to the host.  Uses the RX interrupt

//          to receive characters.

//

//    SCIB: Host, known baud rate, sends characters to the slave

//          and checks that they are echoed back.

//

// DESCRIPTION:

//

//    Internal Loopback test for ever through SCIA using interrupts,

//   FIFOs are disabled.

//

//    Watch Variables: BRRVal - current BRR value used for SCIB

//                     ReceivedAChar - character received by SCIA

//                     ReceivedBChar - character received by SCIB

//                     SendChar      - character being sent by SCIB

//                     SciaRegs.SCILBAUD - SCIA baud registers - set

//                     SciaRegs.SCIHBAUD   by autobaud lock

//

//

//###########################################################################

// $TI Release: DSP280x C/C++ Header Files V1.70 $

// $Release Date: July 27, 2009 $

//###########################################################################

#include "DSP280x_Device.h"     // DSP280x Headerfile Include File

#include "DSP280x_Examples.h"   // DSP280x Examples Include File

#define BAUDSTEP 100            // Amount BRR will be incremented between each

                                // autobaud lock

// Prototype statements for functions found within this file.

void scia_init(void);

void scib_init(void);

void scia_xmit(int a);

void scib_xmit(int a);

void scia_AutobaudLock(void);

void error();

interrupt void rxaint_isr(void);

// Global counts used in this example

Uint16 LoopCount;

//Uint16 xmitCount;

Uint16 ReceivedCount;

Uint16 ErrorCount;

Uint16 SendChar;

Uint16 ReceivedAChar;   // scia received character

Uint16 ReceivedBChar;   // scib received character

Uint16 BRRVal;

Uint16 Buff[10] = {0x55, 0xAA, 0xF0, 0x0F, 0x00, 0xFF, 0xF5, 0x5F, 0xA5, 0x5A};

void main(void)

{

   Uint16 i;

// Step 1. Initialize System Control:

// PLL, WatchDog, enable Peripheral Clocks

// This example function is found in the DSP280x_SysCtrl.c file.

   InitSysCtrl();

// Step 2. Initalize GPIO:

// This example function is found in the DSP280x_Gpio.c file and

// illustrates how to set the GPIO to it's default state.

// InitGpio();  // Skipped for this example

   InitSciGpio();

// Initialize PIE control registers to their default state.

// The default state is all PIE interrupts disabled and flags

// are cleared.

// This function is found in the DSP280x_PieCtrl.c file.

   InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:

   IER = 0x0000;

   IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt

// Service Routines (ISR).

// This will populate the entire table, even if the interrupt

// is not used in this example.  This is useful for debug purposes.

// The shell ISR routines are found in DSP280x_DefaultIsr.c.

// This function is found in DSP280x_PieVect.c.

   InitPieVectTable();

// Interrupts that are used in this example are re-mapped to

// ISR functions found within this file.

   EALLOW;     // This is needed to write to EALLOW protected registers

   PieVectTable.SCIRXINTA = &rxaint_isr;

   EDIS;       // This is needed to disable write to EALLOW protected register

// Step 4. Initialize all the Device Peripherals:

// This function is found in DSP280x_InitPeripherals.c

// InitPeripherals(); // Not required for this example

   scia_init();       // Initalize SCIA

   scib_init();       // Initalize SCIB

// Step 5. User specific code, enable interrupts:

   LoopCount = 0;

   ErrorCount = 0;

// Enable interrupts

   PieCtrlRegs.PIEIER9.all = 0x0001; // Enable all SCIA RXINT interrupt

   IER |= 0x0100;         // enable PIEIER9, and INT9

   EINT;

    // Start with BRR = 1, work through each baud rate setting

    // incrementing BRR by BAUDSTEP

    for (BRRVal = 0x0000; BRRVal < (Uint32)0xFFFF; BRRVal+=BAUDSTEP)

    {

        // SCIB has a known baud rate.  SCIA will autobaud to match

    ScibRegs.SCIHBAUD = (BRRVal >> 8);

    ScibRegs.SCILBAUD = (BRRVal);

    // Initiate an autobaud lock with scia.  Check

    // returned character against baud lock character 'A'

    scia_AutobaudLock();

    while(ScibRegs.SCIRXST.bit.RXRDY != 1) { }

    ReceivedBChar = 0;

    ReceivedBChar =  ScibRegs.SCIRXBUF.bit.RXDT;

    if(ReceivedBChar != 'A')

    {

        error(0);

    }

    // Send/echoback characters

    // 55 AA F0 0F 00 FF F5 5F A5 5A

    for(i= 0; i<=9; i++)

    {

      SendChar = Buff[i];

      scib_xmit(SendChar);     // Initiate interrupts and xmit data in isr

      // Wait to get the character back and check

      // against the sent character.

      while(ScibRegs.SCIRXST.bit.RXRDY != 1)

      {

          asm("   NOP");

      }

      ReceivedBChar = 0;

      ReceivedBChar =  ScibRegs.SCIRXBUF.bit.RXDT;

      if(ReceivedBChar != SendChar) error(1);

    }

    } // Repeat for next BRR setting

    // Stop here, no more

    for(;;)

    {

       asm("    NOP");

    }

}

/* --------------------------------------------------- */

/* ISR for PIE INT9.1                                  */

/* Connected to RXAINT  SCI-A                          */

/* ----------------------------------------------------*/

interrupt void rxaint_isr(void)     // SCI-A

{

  // Insert ISR Code here

   PieCtrlRegs.PIEACK.all = PIEACK_GROUP9;

   // If autobaud detected, we must clear CDC and ABD.

   if(SciaRegs.SCIFFCT.bit.ABD == 1)

   {

      SciaRegs.SCIFFCT.bit.ABDCLR = 1;

      SciaRegs.SCIFFCT.bit.CDC = 0;

      // Check received character - should be 'A'

      ReceivedAChar = 0;

      ReceivedAChar = SciaRegs.SCIRXBUF.all;

      if(ReceivedAChar != 'A')

      {

         error(2);

      }

      else scia_xmit(ReceivedAChar);

   }

   // This was not autobaud detect

   else

   {

      // Check received character against sendchar

      ReceivedAChar = 0;

      ReceivedAChar = SciaRegs.SCIRXBUF.all;

      if(ReceivedAChar != SendChar)

      {

         error(3);

      }

      else scia_xmit(ReceivedAChar);

   }

   SciaRegs.SCIFFRX.bit.RXFFINTCLR = 1; // clear Receive interrupt flag

   ReceivedCount++;

}

void error()

{

      ErrorCount++;

      asm("     ESTOP0");         // Uncomment to stop the test here

      for (;;);

}

// SCIA  8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity

void scia_init()

{

    // Note: Clocks were turned on to the SCIA peripheral

    // in the InitSysCtrl() function

    // Reset FIFO's

    SciaRegs.SCIFFTX.all=0x8000;

    SciaRegs.SCICCR.all =0x0007;   // 1 stop bit,  No loopback

                                   // No parity,8 char bits,

                                   // async mode, idle-line protocol

    SciaRegs.SCICTL1.all =0x0003;  // enable TX, RX, internal SCICLK,

                                   // Disable RX ERR, SLEEP, TXWAKE

    SciaRegs.SCICTL2.all =0x0003;

    SciaRegs.SCICTL2.bit.RXBKINTENA =1;

    SciaRegs.SCICTL1.all =0x0023;     // Relinquish SCI from Reset

}

// SCIB  8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity

void scib_init()

{

    // Reset FIFO's

    ScibRegs.SCIFFTX.all=0x8000;

    // 1 stop bit, No parity, 8-bit character

    // No loopback

    ScibRegs.SCICCR.all = 0x0007;

    // Enable TX, RX, Use internal SCICLK

    ScibRegs.SCICTL1.all = 0x0003;

    // Disable RxErr, Sleep, TX Wake,

    // Diable Rx Interrupt, Tx Interrupt

    ScibRegs.SCICTL2.all = 0x0000;

    // Relinquish SCI-A from reset

    ScibRegs.SCICTL1.all = 0x0023;

    return;

}

// Transmit a character from the SCI-A'

void scia_xmit(int a)

{

    SciaRegs.SCITXBUF=a;

}

// Transmit a character from the SCI-B'

void scib_xmit(int a)

{

    ScibRegs.SCITXBUF=a;

}

//------------------------------------------------

// Perform autobaud lock with the host.

// Note that if autobaud never occurs

// the program will hang in this routine as there

// is no timeout mechanism included.

//------------------------------------------------

void scia_AutobaudLock()

{

   

    SciaRegs.SCICTL1.bit.SWRESET = 0;

    SciaRegs.SCICTL1.bit.SWRESET = 1;

    // Must prime baud register with >= 1

    SciaRegs.SCIHBAUD = 0;

    SciaRegs.SCILBAUD = 1;

    // Prepare for autobaud detection

    // Make sure the ABD bit is clear by writing a 1 to ABDCLR

    // Set the CDC bit to enable autobaud detection

    SciaRegs.SCIFFCT.bit.ABDCLR = 1;

    SciaRegs.SCIFFCT.bit.CDC = 1;

    // Wait until we correctly read an

    // 'A' or 'a' and lock

//

// As long as Autobaud calibration is enabled (CDC = 1),

// SCI-B (host) will continue transmitting 'A'. This will

// continue until interrupted by the SCI-A RX ISR, where

// SCI-A RXBUF receives 'A', autobaud-locks (ABDCLR=1

// CDC=0),and returns an 'A' back to the host. Then control

// is returned to this loop and the loop is exited.

//

// NOTE: ABD will become set sometime between 

//       scib_xmit and the DELAY_US loop, and

//       the SCI-A RX ISR will be triggered.

    //       Upon returning and reaching the if-statement,

//       ABD will have been cleared again by the ISR.

    while(SciaRegs.SCIFFCT.bit.CDC== 1) 

    {  

       // Note the lower the baud rate the longer

       // this delay has to be to allow the other end

       // to echo back a character (about 4 characters long)

       // Make this really long since we are going through all

       // the baud rates.

       DELAY_US(280000L);

       if(SciaRegs.SCIFFCT.bit.CDC == 1)  

           scib_xmit('A');  // host transmits 'A' 

   }

    return;

}

//===========================================================================

// No more.

//===========================================================================