This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
发现我通过Expressions观测到的ClkCfgRegs.SYSPLLSTS.bit.LOCKS的值为0,但是通过Regisrers观测到ClkCfgRegs.SYSPLLSTS.bit.LOCKS的值为1。并且程序无法锁住,请问这是什么原因,如何去解决?望回复,谢谢!
工程师已经回复了:
Please have customer try an example from the latest version of C2000ware (3_02_00_00). Please run the example "as is" without any modification and verify if this problem is seen. I recommend something simple like the CPU Timer test case or GPIO toggle in C:\ti\c2000\C2000Ware_3_02_00_00\driverlib\f2837xd\examples\cpu1.