代码如下:
//#############################################################################
//
// FILE: spi_ex2_dma_loopback.c
//
// TITLE: SPI Digital Loop Back with DMA Example.
//
//! \addtogroup bitfield_example_list
//! <h1>SPI Digital Loop Back with DMA (spi_loopback_dma)</h1>
//!
//! This program uses the internal loop back test mode of the peripheral.
//! Other then boot mode pin configuration, no other hardware configuration
//! is required. Both DMA Interrupts and the SPI FIFOs are used.
//!
//! A stream of data is sent and then compared to the received stream.
//! The sent data looks like this: \n
//! 0000 0001 \n
//! 0001 0002 \n
//! 0002 0003 \n
//! .... \n
//! 007E 007F \n
//!
//! \b Watch \b Variables \n
//! - \b sdata - Data to send
//! - \b rdata - Received data
//! - \b rdata_point - Used to keep track of the last position in
//! the receive stream for error checking
//!
//
//#############################################################################
// $TI Release: F28004x Support Library v1.06.00.00 $
// $Release Date: Mon May 27 06:42:25 CDT 2019 $
// $Copyright:
// Copyright (C) 2019 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################
//
// Included Files
//
#include "F28x_Project.h"
//
// Defines
//
#define BURST (FIFO_LVL-1) // burst size should be less than 8
#define TRANSFER 15 // [(MEM_BUFFER_SIZE/FIFO_LVL)-1]
#define FIFO_LVL 8 // FIFO Interrupt Level
//
// Globals
//
#pragma DATA_SECTION(sdata, "ramgs0"); // map the TX data to memory
#pragma DATA_SECTION(rdata, "ramgs1"); // map the RX data to memory
uint16_t sdata[128]; // Send data buffer
uint16_t rdata[128]; // Receive data buffer
uint16_t rdata_point; // Keep track of where we are
// in the data stream to check received data
volatile uint16_t *DMADest;
volatile uint16_t *DMASource;
volatile uint16_t done;
//
// Function Prototypes
//
__interrupt void local_D_INTCH5_ISR(void);
__interrupt void local_D_INTCH6_ISR(void);
void dma_init(void);
void spi_fifo_init(void);
void error();
//
// Main
//
void main(void)
{
uint16_t i;
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f28004x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the f28004x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// Setup only the GP I/O only for SPI-A functionality
// This function is found in f28004x_Spi.c
//
// InitSpiaGpio();
//
// Step 3. Clear all interrupts:
//
DINT;
//
// Initialize PIE control registers to their default state.
// The default state is all PIE __interrupts disabled and flags
// are cleared.
// This function is found in the f28004x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU __interrupts and clear all CPU __interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in f28004x_DefaultIsr.c.
// This function is found in f28004x_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.DMA_CH5_INT= &local_D_INTCH5_ISR;
PieVectTable.DMA_CH6_INT= &local_D_INTCH6_ISR;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize the Device Peripherals:
//
dma_init();
spi_fifo_init(); // Initialize the SPI FIFO
//
// Ensure DMA is connected to Peripheral Frame 2 bridge (EALLOW protected)
//
//
// Step 5. User specific code:
//
//
// Initialize the data buffers
//
for(i=0; i<128; i++)
{
sdata[i] = i;
rdata[i]= 0;
}
rdata_point = 0;
//
// Enable interrupts required for this example
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
PieCtrlRegs.PIEIER7.bit.INTx5 = 1; // Enable PIE Group 7, INT 1 (DMA CH1)
PieCtrlRegs.PIEIER7.bit.INTx6 = 1; // Enable PIE Group 7, INT 2 (DMA CH2)
IER= M_INT7; // Enable CPU INT6
EINT; // Enable Global Interrupts
StartDMACH6(); // Start SPI RX DMA channel
StartDMACH5(); // Start SPI TX DMA channel
done = 0; // Test is not done yet
while(!done); // wait until the DMA transfer is complete
//
// when the DMA transfer is complete the program will stop here
//
ESTOP0;
}
//
// error - Halt debugger when error received
//
void error(void)
{
asm(" ESTOP0"); //Test failed!! Stop!
for (;;);
}
//
// spi_fifo_init - Initialize SPIA FIFO
//
void spi_fifo_init()
{
//
// Initialize SPI FIFO registers
//
SpiaRegs.SPIFFRX.all=0x2040; // RX FIFO enabled, clear FIFO int
SpiaRegs.SPIFFRX.bit.RXFFIL = FIFO_LVL; // Set RX FIFO level
SpiaRegs.SPIFFTX.all=0xE040; // FIFOs enabled, TX FIFO released,
SpiaRegs.SPIFFTX.bit.TXFFIL = FIFO_LVL; // Set TX FIFO level
//
// InitSpi();
//
SpiaRegs.***.bit.SPISWRESET = 0;
SpiaRegs.***.bit.CLKPOLARITY = 0;
SpiaRegs.***.bit.*** = (16 - 1);
SpiaRegs.***.bit.SPILBK = 1;
SpiaRegs.***.bit.MASTER_SLAVE = 1;
SpiaRegs.***.bit.TALK = 1;
SpiaRegs.***.bit.CLK_PHASE = 0;
SpiaRegs.***.bit.SPIINTENA = 0;
SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = ((25000000 / 1000000) - 1);
SpiaRegs.SPIPRI.bit.FREE = 1;
SpiaRegs.***.bit.SPISWRESET = 1;
}
//
// dma_init - DMA setup for both TX and RX channels.
//
void dma_init()
{
//
// Initialize DMA
//
DMAInitialize();
DMASource = (volatile uint16_t *)sdata;
DMADest = (volatile uint16_t *)rdata;
//
// configure DMACH5 for TX
//
DMACH5AddrConfig(&SpiaRegs.SPITXBUF,DMASource);
DMACH5BurstConfig(BURST,1,0); // Burst size, src step, dest step
DMACH5TransferConfig(TRANSFER,1,0); // transfer size, src step, dest step
DMACH5ModeConfig(DMA_SPIATX,PERINT_ENABLE,ONESHOT_DISABLE,CONT_DISABLE,
SYNC_DISABLE,SYNC_SRC,OVRFLOW_DISABLE,SIXTEEN_BIT,
CHINT_END,CHINT_ENABLE);
//
// configure DMA CH2 for RX
//
DMACH6AddrConfig(DMADest,&SpiaRegs.SPIRXBUF);
DMACH6BurstConfig(BURST,0,1);
DMACH6TransferConfig(TRANSFER,0,1);
DMACH6ModeConfig(DMA_SPIARX,PERINT_ENABLE,ONESHOT_DISABLE,CONT_DISABLE,
SYNC_DISABLE,SYNC_SRC,OVRFLOW_DISABLE,SIXTEEN_BIT,
CHINT_END,CHINT_ENABLE);
}
//
// local_D_INTCH5_ISR - DMA Channel 5 ISR
//
__interrupt void local_D_INTCH5_ISR(void)
{
EALLOW; // NEED TO EXECUTE EALLOW INSIDE ISR !!!
DmaRegs.CH5.CONTROL.bit.HALT=1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP7; // ACK to receive more interrupts
// from this PIE group
EDIS;
return;
}
//
// local_D_INTCH6_ISR - DMA Channel 6 ISR
//
__interrupt void local_D_INTCH6_ISR(void)
{
uint16_t i;
EALLOW; // NEED TO EXECUTE EALLOW INSIDE ISR !!!
DmaRegs.CH6.CONTROL.bit.HALT = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP7; // ACK to receive more interrupts
// from this PIE group
EDIS;
for( i = 0; i<128; i++ )
{
//
// check for data integrity
//
if(rdata[i] != i)
{
error();
}
}
done = 1; // test done.
return;
}
//
// End of File
//