This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
小弟第一次在網上發問,想請問各位高手問題,希望能幫忙解惑。
最近小弟在研究TMS320F28379D的SDFM模塊,使用AMC1304的module,功能是感測無感電阻的電壓,經過轉換再給到DSP。
AMC1304的module與DSP之間連結我是用2條線接起來(AMC1304 module 選一組CLK與DATA)(DSP分別是SD1_D1和SD1_C1接腳),然後我DSP程式部分使用的是範例程式 "sdfm_pwm_sync_cpu",下面我遇到的狀況:
我想請教的是,會跳開是我AMC1304的module與DSP配線問題,還是哪邊沒設定好,不知道小弟哪裡沒考慮到,希望版上的高手能撥時間幫小弟解惑。
額外問個問題,我在查GPIO的表看到SD1_D1和SD1_C1都是算(I)的設定,所以代表說還要從哪裡給訊號嗎?
你好,我看了一下AMC1304的CLK引脚,AMC1304和C2000 内部的SINC都是输入的,所以需要一个外部时钟信号来给它们,可以用一个PWM信号。
可以参考一下下面的原理图进行设计: