This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28335 CANTA问题



调试时发现while (ECanaRegs.CANTA.all == 0);卡在这一句了,我的CAN上接了一个USB转CAN的分析仪,可以用作接收节点,请问这是为什么

  • 请问您调试的是例程还是您自己的工程?能否给出相关代码或工程,谢谢
  • 如下是我的配置代码,请帮忙看一下
    struct ECAN_REGS ECanaShadow;
    EALLOW; // EALLOW enables access to protected bits
    GpioCtrlRegs.GPAPUD.bit.GPIO18 = 0; // Enable pull-up for GPIO18 (CANRXA)
    GpioCtrlRegs.GPAPUD.bit.GPIO19 = 1; //Enable pull-up for GPIO19 (CANTXA)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO18 = 3; // Asynch qual for GPIO18 (CANRXA)
    GpioCtrlRegs.GPAMUX2.bit.GPIO18 = 3; // Configure GPIO18 for CANRXA
    GpioCtrlRegs.GPAMUX2.bit.GPIO19 = 3; // Configure GPIO19 for CANTXA

    //配置eCAN的RX和TX分别为eCAN的接收和发送引脚
    ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
    ECanaShadow.CANTIOC.bit.TXFUNC = 1;
    ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;

    ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
    ECanaShadow.CANRIOC.bit.RXFUNC = 1;
    ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;

    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.STM = 0; //工作在正常模式
    ECanaShadow.CANMC.bit.SCB = 1;
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
    //初始化所有主设备控制区域为0,MCF所有的位都初始化为0
    ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
    ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;

    // TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
    // as a matter of precaution.

    ECanaShadow.CANTA.all = ECanaRegs.CANTA.all;
    ECanaShadow.CANTA.all = 0xFFFFFFFF;
    ECanaRegs.CANTA.all = ECanaShadow.CANTA.all;

    ECanaShadow.CANRMP.all = ECanaRegs.CANRMP.all;
    ECanaShadow.CANRMP.all = 0xFFFFFFFF;
    ECanaRegs.CANRMP.all = ECanaShadow.CANRMP.all;


    ECanaShadow.CANGIF0.all = ECanaRegs.CANGIF0.all;
    ECanaShadow.CANGIF0.all = 0xFFFFFFFF;
    ECanaRegs.CANGIF0.all = ECanaShadow.CANGIF0.all;

    ECanaShadow.CANGIF1.all = ECanaRegs.CANGIF1.all;
    ECanaShadow.CANGIF1.all = 0xFFFFFFFF;
    ECanaRegs.CANGIF1.all = ECanaShadow.CANGIF1.all;

    /* Configure bit timing parameters for eCANB*/

    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;

    ECanaShadow.CANES.all = ECanaRegs.CANES.all;
    do
    {
    ECanaShadow.CANES.all=ECanaRegs.CANES.all;
    }while (ECanaShadow.CANES.bit.CCE != 1 ) ; // Wait for CCE bit to be set..


    ECanaShadow.CANBTC.all = ECanaRegs.CANBTC.all;
    ECanaShadow.CANBTC.bit.BRPREG = 9;
    /*150/10=15*/
    ECanaShadow.CANBTC.bit.TSEG2REG = 2;
    ECanaShadow.CANBTC.bit.TSEG1REG = 10;
    ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;

    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;

    do
    {
    ECanaShadow.CANES.all = ECanaRegs.CANES.all;
    }while (ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..


    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.all = 0; // Required before writing the MSGIDs
    ECanaRegs.CANME.all = ECanaShadow.CANME.all;

    /*发送邮箱的ID号*/
    ECanaMboxes.MBOX0.MSGID.all = 0x00C80000;
    /*接收邮箱的ID号*/
    ECanaMboxes.MBOX16.MSGID.all = 0x00C80000;

    /*邮箱0为TX,16为RX*/
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.bit.MD0 =0;
    ECanaShadow.CANMD.bit.MD16 =1;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;

    /*数据长度 8个BYTE*/
    ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
    ECanaMboxes.MBOX16.MSGCTRL.bit.DLC = 8;

    //设置发送优先级 2009.3.15 Add
    ECanaMboxes.MBOX0.MSGCTRL.bit.TPL = 0;
    ECanaMboxes.MBOX16.MSGCTRL.bit.TPL = 0;

    /*没有远方应答帧被请求*/
    ECanaMboxes.MBOX0.MSGCTRL.bit.RTR = 0;
    ECanaMboxes.MBOX16.MSGCTRL.bit.RTR = 0;

    //向邮箱RAM区写数据
    ECanaMboxes.MBOX0.MDL.all = 0x01234567;
    ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;

    //邮箱使能Mailbox0
    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.bit.ME0 =1;
    ECanaShadow.CANME.bit.ME16 =1;
    ECanaRegs.CANME.all = ECanaShadow.CANME.all;

    EDIS;
  • 您的 while (ECanaRegs.CANTA.all == 0); 是在哪里处理的?若是可以的话,还是请您私信工程,谢谢

    现在28335用作接收节点,使用CAN测试软件来发送can数据?
  • 现在是两个板子用CAN通讯,一个是发送节点,一个是接收节点,我现在私信您工程
  • 不好意思,私信贴不过去,我贴在这里can_tx.zip

  • 参考您最新的帖子 e2echina.ti.com/.../195076

    现在可以发送了?
  • 是可以发送了,是因为我接收节点没有处理好,导致卡在判断那里
  • 好的 谢谢您的反馈