This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

epwm相关问题

看到Ti2000芯片有些芯片具有模式2和模式4,请问那些芯片具有基本的epwm功能,那些芯片具有模式2,那些芯片具有模式4.

 那些芯片的epwm动作寄存器具有影子寄存器。

  • 你好,方便更详细描述一下模式2模式4是指什么的模式吗?
    影子寄存器的话几乎所有C2000系列芯片的ePWM模块都有影子寄存器。
  • Introduction
    This chapter includes an overview of the module and information about each of its submodules:
    • Time-Base Module
    • Counter Compare Module
    • Action Qualifier Module
    • Dead-Band Generator Module
    • PWM Chopper (PC) Module
    • Trip Zone Module
    • Event Trigger Module
    • Digital Compare Module
    The ePWM Type 4 is functionally compatible to the Type 2 module (a Type 3 does not exist). Type 4 has
    the following enhancements in addition to the Type 2 features:


    14.6.4 AQCTLA and AQCTLB Shadow Mode Operations
    To enable Action Qualifier mode changes which must occur at the end of a period even when the phase
    changes, shadowing of the AQCTLA and AQCTLB registers has been added on ePWMs type 2 and later.
    Additionally, shadow to active load on SYNC of these registers is supported as well. Shadowing of this
    register is enabled and disabled by the AQCTLR[SHDWAQAMODE] and AQCTLR[SHDWAQBMODE]
    bits. These bits enable and disable the AQCTLA shadow register and AQCTLB shadow register,

    TMS320F377D 手册中提到type4、type2,另外提到了AQCTLA和AQCTLB具有影子操作模式。我想请教一下,除了377D这个芯片外,其他2000系列的芯片那些还具有type4和type2,哪些AQCTLA和AQCTLB具有影子操作模式。因为我之前看28335好像是没有这些模式的。
  • 你好,关于C2000系列PWM的区别问题,可以参考以下文档第35页:www.ti.com/.../spru566n.pdf
  • 你好,关于TI2000DSP用在三电平变流器NPC拓扑结构的一些应用,有没有想过的介绍或说明的文档,介绍如何使用EPWM模块实现三电平的发波设置。
    多谢!
  • 目前TI还没有开发类似的应用。