This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问一下关于 TMS320F240 DSP-Solution for HighResolution Position with Sin/CosEncoders 文档反正切表问题



你好 请问一下 

https://www.ti.com/lit/an/spra496/spra496.pdf

  这个文档的第 37页开始 Q15_ATAN.INC 文档里面的 反正切表的生成方法  我想改一个 Q10格式的 

  • 我不太明白 这个表是怎么生成的   方便告诉我嘛 谢谢

  • 我会在确认后给您回复,谢谢
  • 请您参考下面链接内的回复

    e2e.ti.com/.../3530527

    thank you for your interest in the Application Report SPRA496.

    I wrote the Assembly code only for Q15 fractional numbers. The function "int q15p_atan(int)" returns the angle scaled by PI in the range from 0 to PI/4. Hence the return value 0x000 = 0.0 (Q15) equals 0 degree and 0x2000 = 0.25 (Q15) equals PI/4 (45 degree). The Q15 gives the highest possible resolution, as also the input argument is scaled as Q15 from 0 to 0x7FFF (0.999).

    Unfortunately I won't be able to rewrite the TMS320F240 Assembly code to Q10 format anymore.

    However you may change yourself. Then you may consider the product shift mode SPM.

    The code I used is written for SPM=1 (see assembly instruction) to handle Q15xQ15=Q30. With the automatic product shift mode (SPM 1) the product is automatically left shifted by 1 bit = Q31 so the resulting Q15 number is in the upper 16-bit of the 32-bit ACC (store ACCH).

    When you go for Q10 then a multiplication product gives you Q10xQ10=Q20. To get a Q10 equivalent result in the upper 16-bit of the ACC you need an product shift mode by 11. I think SPM 11 is not supported by the F240 DSP core, but please check. Another option to get a Q10 results: You can instead right shift the 32-bit intermediate results by 10 so the Q10 scaled product is in the lower 16-bit of the ACC. In that case SPM needs to be 0. But please be aware you may get overflow as Q10xQ10 can exceed the Q10 range of +/-32.0.
  • 若是您有更进一步的问题,请在之前的英文贴内继续跟帖回复

    e2e.ti.com/.../3530527
  • Hello:
    Thank you for your answers,
    1 >.
    I don't know if that's right
    The 0-0.99 Q15 format corresponds to 0-32768
    The 0-0.25 Q15 format corresponds to the 0-pi / 4-> 0-8192 45 degree subdivision into 128 pieces
    45/128 = 0.3515625 degree
    table degree[129] =
    {
    0,
    0.3515625,
    .
    .
    .
    ..
    44.6484375,
    45
    }
    2 >.
    Here is SPRA496 document Q15_ATAN
    table[129]={
    0
    ,81,163,244,326,407,489,570,651,
    732,813,894,975,1056,1136,1217,1297,
    1377,1457,1537,1617,1696,1775,1854,1933,
    2012,2090,2168,2246,2324,2401,2478,2555,
    2632,2708,2784,2860,2935,3010,3085,3159,
    3233,3307,3380,3453,3526,3599,3670,3742,
    3813,3884,3955,4025,4095,4164,4233,4302,
    4370,4438,4505,4572,4639,4705,4771,4836,
    4901,4966,5030,5094,5157,5220,5282,5344,
    5406,5467,5528,5589,5649,5708,5768,5826,
    5885,5943,6000,6058,6114,6171,6227,6282,
    6337,6392,6446,6500,6554,6607,6660,6712,
    6764,6815,6867,6917,6968,7018,7068,7117,
    7166,7214,7262,7310,7358,7405,7451,7498,
    7544,7589,7635,7679,7724,7768,7812,7856,
    7899,7942,7984,8026,8068,8110,8151,8192,
    }
    I don't understand table[1] = 81?table[1] = 163 ?
    table[127] = 8151?
    What is the generation pattern of the above table elements?
    How is this part of the value generated

    thank you
  • 已经在下面链接内回复了,您可以跟踪一下

    e2e.ti.com/.../3532481
  • the atan(x), where x can be from 0 to 1.0, is a nonlinear function and as as such the lookup table is nonlinear too. The lookup table is basically an 8-bit approximation of the atan(x) function. The argument x is right shifted to get an 8-bit equivalent pointer to the corresponding approximate angle value in the lookup table.

    Example:

    atan(0): 0 is converted to 0 and points to the first element in the lookup table: 0

    atan(1.0): 1.0 is converted to 128 and points to the last (129) element in the lookup table: 8192=0.25 Q15 (equals PI*0.25=45deg)

    atan(0.5): 0.5 is converted to 64 and points to the 65 element in the lookup table: 4836=0.149 Q15 (equals P*0.1475= 26.56deg)

    atan(0.25): 0.25 is converted to 32 and points to the 33 element in the lookup table: 2555=0.077 Q15 (equals P*0.077= 14.03deg)

    and so on.