This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28388D的SPI



目前想通过SPI外扩NOR   FLASH,SPI接口的NOR  FLASH的数据位分为:一位、两位、四位、八位。如果我想数据传输的速度足够快,数据位数就需要尽可能的多。

查阅28388D的手册发现,28388D有4路SPI,每一路有4根线,4根线中有两根数据线(SIMO、SOMI)、一根时钟线(SPI_CLK)和一根从机发送使能线SPI_STEn),

选择的NOR  FLASH是如下图所示:

NOR   FLASH中有效引脚是9根,9根中有4根数据线,我想要的是,数据的传输速度最快,所以NOR   FLASH的4根数据线,应该要同时和28388D的SPI进行数据传输。

但是,硬件上只有两根数据线,另外两根的话,是要接到哪里呢?

我思考着,是将另外的两根数据线接到28388D的GPIO上,但是,这样接的话,会存在普通引脚当数据线使用的情况,所以一时间,不知道如何解决了,特来请教28388D的SPI接口,是如何和外扩的FLASH进行数据传输和接线的呢。

还有人,是将DQ2和DQ3用3.3V拉高,这样的话,就没办法使用NOR   FLASH上面的4根数据线进行传输了。