This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] LAUNCHXL-F28069M无法识别USB串行端口的解决方法



某些LAUNCHXL-F28069M板上的XDS100 USB串行端口可能未正确配置。这种情况的显示为Windows无法识别USB串行端口。下面是在设备管理器中正确识别的XDS100 USB串行端口的情况:

如果您的LAUNCHXL-F28069M上未标识串行端口,则  可以使用以下步骤对XDS100 EEPROM进行重新编程:

1从FTDI 下载  MPROG 3.5

2 解压并运行MPROG

3 将LaunchPad连接到PC

4 Device >> Scan找到您的XDS100

5 Tools >> Read and Parse以解码您的编程设置(仅在满足以下条件时继续)

1)产品说明包括XDS100

2)Side B驱动程序设置为D2XX Direct,而不是虚拟COM端口

6 File >> Save As(用于备份)

7 File >> Edit 

8 将Side B驱动程序更新为RS232 UART + Virtual COM Port

9 File >> Save As(您的选择)

10 Device >> Erase

11 Device >> Program

12 拔下LaunchPad

13 再次插入LaunchPad

完成上述步骤后,应在设备管理器中识别您的USB串行端口。

参考链接:e2e.ti.com/.../670519