Other Parts Discussed in Thread: TLV5638
问题:DA型号为TLV5638 附件有具体的问题描述即程序配图,配置完DA程序后用示波器观测到DA有输入信号,但是没有输出信号。请问该如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV5638
问题:DA型号为TLV5638 附件有具体的问题描述即程序配图,配置完DA程序后用示波器观测到DA有输入信号,但是没有输出信号。请问该如何解决?
你好,要更新两个DAC,请按照以下步骤操作,并可以相应地编写代码:
假设你要使用1.024V的内部基准电压,并且要同时更新DAC A和DACB。
1.将参考电压设置为1,024 V(控制寄存器)

2.将DAC B的数据写入BUFFER

3.写入新的DAC A值并同时更新DAC A和B

在从DAC A采样到D0数据字之后,两个输出均在时钟上升沿更新。