This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035 CLK TASK 中无法对EPwm1Regs.CMPA.half.CMPA赋值

我的CLA task 是epwm触发,读取AdcResult.ADCRESULT6数值后,进行运算,得到的结果赋值给EPwm1Regs.CMPA.half.CMPA。

编译没有错误,可以烧写,可以运行,在expressions窗口可以观察到task中其他变量都如期变化,只有CMPA的数值始终是初始化时的给定值。

可能是哪里的配置出了问题呢?

一、CLA配置

/*
 * Cpu_Cla.c
 *
 *  Created on: 2020年11月24日
 *      Author: 29458
 */

#include "DSP28x_Project.h"
#include "Cpu_Cla.h"//所有 CLA中断都定义在Cpu_Cla.h当中
#include "DSP2803x_Examples.h"
#include "string.h"
//Linker defined vars
extern Uint16 Cla1Prog_Start;
extern Uint16 Cla1funcsLoadStart;
extern Uint16 Cla1funcsLoadEnd;
extern Uint16 Cla1funcsRunStart;
extern Uint16 Cla1funcsLoadSize;
extern Uint16 Cla1mathTablesLoadStart;
extern Uint16 Cla1mathTablesRunStart;
extern Uint16 Cla1mathTablesLoadSize;
void Cla_AppInit(void)
{
   /*  Assign user defined ISR to the PIE vector table */
    EALLOW;
   PieVectTable.CLA1_INT1  = &cla1_task1_isr;//取中断向量的地址.放入CPU中断向量表中。
   PieVectTable.CLA1_INT2  = &cla1_task2_isr;
   PieVectTable.CLA1_INT3  = &cla1_task3_isr;
   PieVectTable.CLA1_INT4  = &cla1_task4_isr;
   PieVectTable.CLA1_INT5  = &cla1_task5_isr;
   PieVectTable.CLA1_INT6  = &cla1_task6_isr;
   PieVectTable.CLA1_INT7  = &cla1_task7_isr;
   PieVectTable.CLA1_INT8  = &cla1_task8_isr;
    EDIS;

   //Copy over the CLA code and Tables
   memcpy(&Cla1funcsRunStart, &Cla1funcsLoadStart, (Uint32)&Cla1funcsLoadSize);//将CLA代码拷贝入CLA的代码段,因为CLA的代码需要单独放在一个固定的位置,所以需要执行这一段代码
   memcpy(&Cla1mathTablesRunStart, &Cla1mathTablesLoadStart, (Uint32)&Cla1mathTablesLoadSize);

   /*  Compute all CLA task vectors */
   EALLOW;
   Cla1Regs.MVECT1 = (Uint16)((Uint32)&Cla1Task1 - (Uint32)&Cla1Prog_Start);//取task初始地址的偏移量
   Cla1Regs.MVECT2 = (Uint16)((Uint32)&Cla1Task2 - (Uint32)&Cla1Prog_Start);
   Cla1Regs.MVECT3 = (Uint16)((Uint32)&Cla1Task3 - (Uint32)&Cla1Prog_Start);
   Cla1Regs.MVECT4 = (Uint16)((Uint32)&Cla1Task4 - (Uint32)&Cla1Prog_Start);
   Cla1Regs.MVECT5 = (Uint16)((Uint32)&Cla1Task5 - (Uint32)&Cla1Prog_Start);
   Cla1Regs.MVECT6 = (Uint16)((Uint32)&Cla1Task6 - (Uint32)&Cla1Prog_Start);
   Cla1Regs.MVECT7 = (Uint16)((Uint32)&Cla1Task7 - (Uint32)&Cla1Prog_Start);
   Cla1Regs.MVECT8 = (Uint16)((Uint32)&Cla1Task8 - (Uint32)&Cla1Prog_Start);
   EDIS;

   //  Step 3 : Mapping CLA tasks
   /*  All tasks are enabled and will be started by an ePWM trigger
    *  Map CLA program memory to the CLA and enable software breakpoints
    */
   EALLOW;
   Cla1Regs.MPISRCSEL1.bit.PERINT1SEL     = CLA_INT1_EPWM1INT;//PWM触发CLA的task
   Cla1Regs.MPISRCSEL1.bit.PERINT2SEL     = CLA_INT2_NONE;    //软件触发进入
//   Cla1Regs.MPISRCSEL1.bit.PERINT3SEL     = CLA_INT3_EPWM3INT;
//   Cla1Regs.MPISRCSEL1.bit.PERINT4SEL     = CLA_INT4_EPWM4INT;
//   Cla1Regs.MPISRCSEL1.bit.PERINT5SEL     = CLA_INT5_EPWM5INT;
//   Cla1Regs.MPISRCSEL1.bit.PERINT6SEL     = CLA_INT6_EPWM6INT;
//   Cla1Regs.MPISRCSEL1.bit.PERINT7SEL     = CLA_INT7_EPWM7INT;
//   Cla1Regs.MPISRCSEL1.bit.PERINT8SEL     = CLA_INT8_NONE;
   Cla1Regs.MIER.all                      = 0x00FF;//1111 1111 。配置完成,使能task
   EDIS;

   /*  Enable CLA interrupts at the group and subgroup levels */
   PieCtrlRegs.PIEIER11.all       = 0x0;//中断向量表第11组全部使能
   IER |= M_INT11 ;                        //IER与0100 0000 0000按位或

   /* Switch the CLA program space to the CLA and enable software forcing
    * Also switch over CLA data ram 0 and 1
    */
   EALLOW;
   Cla1Regs.MMEMCFG.bit.PROGE     = 1;// CLA program RAM to CLA space将CLA的数据段和程序段都映射到CLA空间
   Cla1Regs.MMEMCFG.bit.RAM1E    = 1;// CLA data RAM to CLA space
   Cla1Regs.MMEMCFG.bit.RAM0E    = 1;
   Cla1Regs.MCTL.bit.IACKE        = 1;//软件触发
//   Cla1Regs.MIER.all             = 0x00FF;//中断配置好以后,使能所有task
   EDIS;
}
//###########################################################################
// CLA ISRs
//###########################################################################
__interrupt void cla1_task1_isr(void)
{//This interrupt will be taken by the main CPU when CLA task 7  completes.
//    Run_Time_End();
//    GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;//清ACK中断,通常用在ISR的最后;使得同组的其他中断能响应。
}

__interrupt void cla1_task2_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}

__interrupt void cla1_task3_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}

__interrupt void cla1_task4_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}

__interrupt void cla1_task5_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}

__interrupt void cla1_task6_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}

__interrupt void cla1_task7_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}

__interrupt void cla1_task8_isr( void)
{
    PieCtrlRegs.PIEACK.bit.ACK11 = 1;
}


二、CLA task

/*
 * Cla_Task1.cla
 *
 *  Created on: 2020年11月25日
 *      Author: 29458
 */
#include "DSP28x_Project.h"
#include "ClaShare.h"
#include "CLAmath.h"
#include "Cpu_Cla.h"
#include "DSP2803x_Device.h"
#include "DSP2803x_Cla_typedefs.h"

//----------------------变量定义---------------------------------------------//
//float             fCorrectDone;
//float             fguzhangwei;  //校零完成标志位和故障标志位
//float             favg;
//float             favg2;
//float             fsum;
//float             fsum2;
//float             fk;//采样128个点
//float             fADerr;
//float             fADerr2;            //电压采样差值和电流采样差值
//====================SOGI相关变量====================================================================//
float           Uac;
float           u_sogi_k ,u_sogi_k_1 ,u_sogi_k_2 ;//输入变量
float           y_sogi_k ,y_sogi_k_1 ,y_sogi_k_2 ;//同相输出正弦波变量
float           y_sogi_qk,y_sogi_qk_1,y_sogi_qk_2;//正交输出正弦波变量
#define         k_sogi    (float)(0.1)
#define         wn        (int)(314)
#define         Ts        (float)(75e-6)
#define         IQ12Coe      (float)(0.0002441406)//2^12
#define         Coe       (float)(0.0078125)//1/128
#define         x         (float)(0.007853981633974)
#define         y         (float)(0.0000616850275068085)
#define         b0        (float)(0.001959617488787)                //同相正弦波公式系数,
#define         qb0       (float)(0.00000769539988327536)           //正交正弦波中,当前拍输入量的系数
#define         qb1       (float)(0.00001539079976655072)            //正交正弦波中,上一拍输入量的系数
#define         qb2       (float)(0.00000769539988327536)           //正交正弦波中,上上一拍输入量的系数
#define         a1        (float)(1.996019201823359)                  //上一拍输出量的系数
#define         a2        (float)(-0.996080765022425)              //上上一拍输出量的系数
float           Yout;
float            sum;
float            sum2;
float     aaaa;
//把要拷贝到RAM里的函数定义到段Cla1Prog
#pragma CODE_SECTION(Cla1Task2, "Cla1Prog");
__interrupt void Cla1Task2(void)
{
    //Part1:数据赋初值
    CorrectDone = 0;
    guzhangwei  = 0;
    avg         = 0;
    avg2        = 0;
    sum            = 0;
    sum2        = 0;
    k            = 0;//采样128个点
    ADerr        = 0;
    ADerr2        = 0;
}
#pragma CODE_SECTION(Cla1Task1, "Cla1Prog");
__interrupt void Cla1Task1(void)
{
    if(CorrectDone==0)     //校零没有完成
    {
//        delay_2(2);
        sum  += sum_cla;//输出电压采样值
        sum2 += sum2_cla;//输出电流采样值
        if(k<128)
        {
           k++;
        }
        if(k==128)
        {
          avg   = sum*Coe;   //右移7位即除以128,取平均值
          avg2  = sum2*Coe;
          ADerr = avg -2048;//和理论值做差
          ADerr2= avg2-2048;//得到0.2I
          CorrectDone=1;   //校零完成标志位置1
        }
    }
    if(CorrectDone==1)  //校零已经完成
    {
//        Uac=(AdcResult.ADCRESULT6-ADerr)*0.0016-3.279;     //数据处理 3.279/4095*2=0.0016  369
        Uac=(sum_cla-ADerr)*0.0016-3.279;     //数据处理 3.279/4095*2=0.0016  369
//        Uac=sum_cla*0.0016-3.279;     //数据处理 3.279/4095*2=0.0016  369
//            I_L=(AdcResult.ADCRESULT5-ADerr2)*0.0016-3.279;    //得到实际电感电流的0.2倍值。0.2I_L
//---------------------------SOGI-----------------------------------------------------//
        u_sogi_k     = Uac;//输入电网电压
        y_sogi_k     = a1*y_sogi_k_1 + a2*y_sogi_k_2 + b0*(u_sogi_k - u_sogi_k_2);//求与电网电压同相的正弦波
        y_sogi_k_2   = y_sogi_k_1;
        y_sogi_k_1   = y_sogi_k;

        y_sogi_qk    = a1*y_sogi_qk_1 + a2*y_sogi_qk_2 + qb0*u_sogi_k + qb1*u_sogi_k_1 + qb2*u_sogi_k_2;//与电网电压正交的正弦波
        y_sogi_qk_2  = y_sogi_qk_1;
        y_sogi_qk_1  = y_sogi_qk;

        u_sogi_k_2   = u_sogi_k_1;
        u_sogi_k_1   = u_sogi_k;

        Yout         = y_sogi_k;
        if(Yout>0.95)
            Yout=0.95;
        if(Yout<-0.95)
            Yout=-0.95;
        aaaa = Yout*750+750;
        EPwm1Regs.CMPA.half.CMPA   =  800;//!!!!!!!!即使直接写一个具体的值,也无法赋值!!!!!!
        EPwm1Regs.CMPB             = -Yout*750+750;
    }
//        EALLOW;
//        EPwm1Regs.ETCLR.bit.INT    = 1;                   //事件触发清除寄存器,清除中断标志位,因为已经响应过这个中断
        //PieCtrlRegs.PIEACK.all   = PIEACK_GROUP1;       //写1,使该位清零。应答下次定时器中断
//        PieCtrlRegs.PIEACK.all     = PIEACK_GROUP3;       //中断应答,必须有这个信号,才能中断 EPWM1
//        EDIS;
}
__interrupt void Cla1Task3 ( void )
{

}
__interrupt void Cla1Task4 ( void )
{

}
__interrupt void Cla1Task5 ( void )
{

}
__interrupt void Cla1Task6 ( void )
{

}
__interrupt void Cla1Task7 ( void )
{

}
__interrupt void Cla1Task8 ( void )
{

}

//===========================================================================
// End of file.
//===========================================================================
//

三、变量定义

/*
 * ClaEntry.c
 *
 *  Created on: 2020年11月26日
 *      Author: 29458
 */
#include "DSP28x_Project.h"
#include "ClaShare.h"

#pragma DATA_SECTION(CorrectDone,"Cla1ToCpuMsgRAM");//CLA中变量,CPU只能读,不能写
float    CorrectDone;

#pragma DATA_SECTION(guzhangwei,"Cla1ToCpuMsgRAM");
float    guzhangwei;

#pragma DATA_SECTION(avg,"Cla1ToCpuMsgRAM");
float    avg;

#pragma DATA_SECTION(avg2,"Cla1ToCpuMsgRAM");
float    avg2;

//#pragma DATA_SECTION(sum2,"Cla1ToCpuMsgRAM");
//float    sum2;


#pragma DATA_SECTION(k,"Cla1ToCpuMsgRAM");
float    k;

#pragma DATA_SECTION(ADerr,"Cla1ToCpuMsgRAM");
float    ADerr;

#pragma DATA_SECTION(ADerr2,"Cla1ToCpuMsgRAM");
float    ADerr2;

四、变零头文件

/*
 * ClaShare.h
 *
 *  Created on: 2020年11月26日
 *      Author: 29458
 */

#ifndef INCLUDE1_CLASHARE_H_
#define INCLUDE1_CLASHARE_H_

extern float    CorrectDone;
extern float    guzhangwei ;
extern float    avg        ;
extern float    avg2       ;
extern float    sum_cla    ;
extern float    sum2_cla   ;
extern float    k           ;
extern float    ADerr       ;
extern float    ADerr2       ;

#endif /* INCLUDE1_CLASHARE_H_ */

  • 你好,我看到你参考过这个帖子:e2echina.ti.com/.../188510
    请问帖子中提到的解决方案是否有测试过?
  • 才解决。是在*.cla文件首端添加#include "DSP2803x_Cla_typedefs.h"。要放在第一行才有效。具体原理不明。谢谢您的回复。

    另,之前在CPU中的程序现在移到CLA task中执行,结果偏差很大。尤其是ADC采样环节(在初始化时,对ADC结果校零:采集128次求平均值,将该平均值和理论值做差。之前误差只有十几,现在居然有三四百。)不知道是什么原因导致的,是PWM模块配置问题吗?您能给些建议吗?还是另开一个帖子?

  • 你好,据我所知,F28035的CLA只能访问ADC模块的结果寄存器。也就是说,采样的值应该跟CLA没关系,CLA只能对采样的数据进行处理。这么看的话,出现问题可能跟采样部分有关,如果ADC是由PWM触发,那确实有可能跟PWM配置会有关。
    你看一下,如果确实有这方面的问题,建议新开一个帖子进行咨询。