This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想实现DSP程序在线升级功能,把out文件转换成hex后,重新烧写到flash中,我按照《Flash2823x_API_Readme》中的步骤操作,但是在调用Flash28232_Erase((SECTORA|SECTORB|SECTORC|SECTORD), &EraseStatus)时,跳不出来,死在这个,不知道什么原因,请问哪里有F28232的在线编程例程,可以参考一下。谢谢
已经找到卡死在Flash28232_Erase的原因,是因为在擦除SECTORC时,进入非法操作中断ILLEGAL_ISR,是什么原因呢?
Status = Flash28232_Erase(SECTORA, &EraseStatus);
Status &= Flash28232_Erase(SECTORB, &EraseStatus);
Status &= Flash28232_Erase(SECTORD, &EraseStatus);
Status &= Flash28232_Erase(SECTORC, &EraseStatus);//引起错误中断
用API例程测试是否也会有这个问题?如果也有,那芯片擦除FLASH的时候需要额外的250mA的电流,可能会因为电压上的不稳定导致这个问题。
进入非法中断的原因一般是因为内核解码错误,如果OUT转HEX后没有烧写好,当执行到0000,FFFF这类指令就会发生ILLEGAL_ISR
这个在下面有详细解释:
micheal
flashAPI的例程如附件,是基于ccsv3.3和4.x以上的工程。还有可能你需要下载controlSUITE软件。
C:\ti\controlSUITE\libs\utilities\flash_api\2823x\28235\v210\example
在这个flashAPI的例程上进行修改,里面包含了擦除编程验证等过程。
Eric
micheal
另外再给你一个F2812的SCI boot 的应用例子,我觉得虽然这个例子不是用在线升级方式,但原理是相同的,只不过它将注流程序用sci boot的方式导进去RAM,而你是将它固定在flash,运行时再copy在RAM中。而F28232又跟F2812很接近,相信对你有些帮助。
Eric