This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8305如何在lab05b例程里修改驱动mos的电流?

Other Parts Discussed in Thread: BOOSTXL-DRV8305EVM, DRV8305

参考BOOSTXL-DRV8305EVM 的板子,使用F28027F做了一个电机驱动板,但更换了其他的MOS;现在跑起来DRV8305芯片发热比较厉害,

1、请问是否是驱动MOS的电流不匹配?

2、如何在lab05b例程里修改DRV8305驱动mos的电流呢?

万分感谢!

  • 这款套件的电流支持最大峰值 20A 的 15A 连续电流输出,不知道你的mos是多大电流?
    关于芯片发热,你可以参考一下这个帖子:e2echina.ti.com/.../370697
  • 您好,感谢回复。

    我指发热的不是MOS管,是DRV8305;

    驱动电流指的是MOS的G极电流,在lab05b这个例程里是如何修改?因为我看DRV8305手册,是可以修改MOS栅极的驱动电流的,但不知道再哪修改,请指点,谢谢!

  • 如果你使用与EVM相同的电流感应电路,则问题不在于电流感应。可以检查一下死区时间是否根据MOSFET设置为正确的值,如果更改了电流或电压感应电路,请根据硬件板在user.h中正确设置以下参数。
    #define USER_IQ_FULL_SCALE_VOLTAGE_V (xx)

    #define USER_VOLTAGE_FILTER_POLE_Hz (xx)

    #define USER_ADC_FULL_SCALE_VOLTAGE_V (xx)

    #define USER_IQ_FULL_SCALE_CURRENT_A (xx)

    #define USER_ADC_FULL_SCALE_CURRENT_A (xx)