This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,28335上电卡死?



28835的板子我已经做过好几次了,之前板子上电运行都正常的,但最近这两块板子遇到了28335上电后VDDIO电压是3.6V-3.8V的问题,无法烧写和运行程序。目前我已经做了一些排查工作,但无法定位问题在哪?请大家帮忙分析分析,多谢!

28335芯片采用301芯片供电和30M的有源晶振。

现象描述:

1.在我不焊接28335芯片时候上电,电源芯片输出的VDDIO和VDD正常,为3.3V和1.9V。

2.焊接28335芯片后上电,VDDIO为3.6V-3.8V,VDD电压正常,为1.9V。此时无法烧写和运行程序。奇怪的是如果我用万用表量晶振时钟信号输出的电压在1.83V左右,量一会后,晶振时钟的输出电压会降到1.76V左右,然后VDDIO电压就回到3.3V了,此时就可以烧写和运行程序。

现在不能确认是否就是晶振电路的问题?然后这问题该如何解决呢?