CAN通信中断使能只能提供 了一个函数
static void CAN_enableInterrupt ( uint32_t base, uint32_t intFlags )
CAN_INT_ERROR - a controller error condition has occurred
CAN_INT_STATUS - a message transfer has completed, or a bus error has been detected
CAN_INT_IE0 - allow CAN controller to generate interrupts on interrupt line 0
CAN_INT_IE1 - allow CAN controller to generate interrupts on interrupt line 1
1、使能IE0意思是所有CAN中断分配到IE0即CAN0INT了?
2、如果只想使能发送中断,不想使能接收中断如何实现
3、发送中断分配到CAN0INT,接收中断分配到CAN1INT如何实现。
4、如果用寄存器编程,CAN的寄存器名称叫什么,就是CAN寄存器那个总的共用体名字。
谢谢帮忙。
主要问题还是库函数不够细致,无法实现复杂的用户自定义,寄存器编程又没例程,连寄存器名字都没公开。好难,比03难用。请提供更多例程。