1、使用的硬件型号:TMDSCNCD28388D – HSEC180 controlCARD
2、使用的例程是: f2838x_cpu1_pdi_hal_test_app
3、位置C:\ti\c2000\C2000Ware_3_03_00_00\libraries\communications\Ethercat\f2838x\examples\f2838x_cpu1_pdi_hal_test_app
4、程序中硬件连接
The controlCARD RJ45 port 0 is connected to PC running TwinCAT master。
5、我的操作:
按照上述,找了根网线,从TMDSCNCD28388D – HSEC180 controlCARD的EtherCAT P0口,接到我的台式机的网口
然后,在台式机上,安装了TwinCAT3.1 ,安装结束,twinCAT3.1被嵌入到VS2017的菜单栏。
6、疑问之处
(1)我的上述操作,是否存在问题
(2)在网上查找了一下,twinCAT3.1被嵌入到VS2017的菜单栏后,如何规范的使用(在调试EtherCAT的时候)。但是没有查到相关资料。
(3)twinCAT3.1,如何搭配例程,进行台式机上的调试使用。
初次调试以太网,特来请教
谢谢!