This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于dsp28335捕捉问题

你好,在dsp28335关于捕捉模块介绍中有这部分内容:

32-Bit Counter and Phase Control

This counter provides the time-base for event captures, and is clocked via the system clock.

A phase register is provided to achieve synchronization with other counters, via a hardware and software

forced sync. This is useful in APWM mode when a phase offset between modules is needed.

我请教一下我如何将要使用的捕捉端口的计数器和外部一个计数器同步起来?能否将捕捉的时基计数器和CPU的T0,T1或者T2计数器同步起来?

  • 你好,我觉得你的理解可能不太对。
    我认为这里的“同步”其实说的是时钟信号的来源。即如果你选择同步信号输入作为时钟信号,那么就可以达到同步的效果。而不是将外部同步信号和芯片本身的计数器同步。