This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28388的M4核:Break at address "0x41c4" with no debug information available, or outside of program code.



你好,我最近在调试28388的M4核,程序从flash启动,目前CpuTimer,UART及其中断都已经调试完成了,都没有问题。现在在调MCAN模块,在调试好的程序基础上添加了C2000提供的MCAN模块例程,单步执行,运行到函数CM_init();// Initialize device clock and peripherals时,进入函数就会报Break at address "0x41c4" with no debug information available, or outside of program code.1,程序一直停留在CM_init()函数的“{”处,请问是什么导致的,谢谢。

一下是我的cmd文件

MEMORY
{
   /* Flash sectors */
   CMBANK0_RESETISR : origin = 0x00200000, length = 0x00000008 /* Boot to Flash Entry Point */
   /*CMBANK0_SECTOR0  : origin = 0x00200008, length = 0x00003FF8
   CMBANK0_SECTOR1  : origin = 0x00204000, length = 0x00004000
   CMBANK0_SECTOR2  : origin = 0x00208000, length = 0x00004000
   CMBANK0_SECTOR3  : origin = 0x0020C000, length = 0x00004000
   CMBANK0_SECTOR4  : origin = 0x00210000, length = 0x00010000
   CMBANK0_SECTOR5  : origin = 0x00220000, length = 0x00010000
   CMBANK0_SECTOR6  : origin = 0x00230000, length = 0x00010000
   CMBANK0_SECTOR7  : origin = 0x00240000, length = 0x00010000
   CMBANK0_SECTOR8  : origin = 0x00250000, length = 0x00010000
   CMBANK0_SECTOR9  : origin = 0x00260000, length = 0x00010000
   CMBANK0_SECTOR10 : origin = 0x00270000, length = 0x00004000
   CMBANK0_SECTOR11 : origin = 0x00274000, length = 0x00004000
   CMBANK0_SECTOR12 : origin = 0x00278000, length = 0x00004000*/
   FLASH_CM        : origin = 0x00200008, length = 0x0007BFF8
   //CMBANK0_SECTOR13 : origin = 0x0027C000, length = 0x00004000
   ParaRom    : origin = 0x0027C000, length = 0x00004000
   /*C1RAM            : origin = 0x1FFFC000, length = 0x00002000
   C0RAM            : origin = 0x1FFFE000, length = 0x00002000*/
   CRAM            : origin = 0x1FFFC000, length = 0x00004000
   BOOT_RSVD        : origin = 0x20000000, length = 0x00000800 /* Part of S0, BOOT rom will use this for stack */
   /*S0RAM            : origin = 0x20000800, length = 0x00003800
   S1RAM            : origin = 0x20004000, length = 0x00004000
   S2RAM            : origin = 0x20008000, length = 0x00004000
   S3RAM            : origin = 0x2000C000, length = 0x00004000
   E0RAM            : origin = 0x20010000, length = 0x00004000*/
   SERAM            : origin = 0x20000800, length = 0x00013800
   CPU1TOCMMSGRAM0  : origin = 0x20080000, length = 0x00000800
   CPU1TOCMMSGRAM1  : origin = 0x20080800, length = 0x00000800
   CMTOCPU1MSGRAM0  : origin = 0x20082000, length = 0x00000800
   CMTOCPU1MSGRAM1  : origin = 0x20082800, length = 0x00000800
   CPU2TOCMMSGRAM0  : origin = 0x20084000, length = 0x00000800
   CPU2TOCMMSGRAM1  : origin = 0x20084800, length = 0x00000800
   CMTOCPU2MSGRAM0  : origin = 0x20086000, length = 0x00000800
   CMTOCPU2MSGRAM1  : origin = 0x20086800, length = 0x00000800
}
SECTIONS
{
   .resetisr        : > CMBANK0_RESETISR
   .vftable         : > FLASH_CM   /* Application placed vector table in Flash*/
   .vtable          : > SERAM             /* Application placed vector table in RAM*/
   .text            : >> FLASH_CM
   .cinit           : > FLASH_CM
   .pinit           : >> FLASH_CM
   .switch          : >> FLASH_CM
   .sysmem          : > SERAM
   .stack           : > CRAM
   .ebss            : > CRAM
   .econst          : >> FLASH_CM
   .esysmem         : > CRAM
   .data            : > SERAM
   .bss             : > SERAM
   .const           : >> FLASH_CM
    MSGRAM_CM_TO_CPU1 : > CMTOCPU1MSGRAM0, type=NOINIT
    MSGRAM_CM_TO_CPU2 : > CMTOCPU2MSGRAM0, type=NOINIT
    MSGRAM_CPU1_TO_CM : > CPU1TOCMMSGRAM0, type=NOINIT
    MSGRAM_CPU2_TO_CM : > CPU2TOCMMSGRAM0, type=NOINIT
 .TI.ramfunc         : LOAD = FLASH_CM,
      RUN = CRAM,
      LOAD_START(TiRamfuncsLoadStart),
      LOAD_SIZE(TiRamfuncsLoadSize),
      LOAD_END(TiRamfuncsLoadEnd),
      RUN_START(TiRamfuncsRunStart),
      RUN_SIZE(TiRamfuncsRunSize),
      RUN_END(TiRamfuncsRunEnd),
      ALIGN(8)
     ramfuncs : {} LOAD = FLASH_CM,
      RUN = SERAM,
      LOAD_START(RamfuncsLoadStart),
      LOAD_SIZE(RamfuncsLoadSize),
      LOAD_END(RamfuncsLoadEnd),
      RUN_START(RamfuncsRunStart),
      RUN_SIZE(RamfuncsRunSize),
      RUN_END(RamfuncsRunEnd),
      ALIGN(8)

}
/*
//===========================================================================
// End of file.
//===========================================================================
*/