This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ICETEK—5100USBV2.0A仿真器通过CCS3.3与板子连接不上



Error connecting to the target:
Error 0x80000200/-1031
Fatal Error during: OCS,
Device driver: Problem with the Emulation Controller.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.


I/O Port = 0

Board Name: F28335 XDS510 Emulator
Cpu Name: CPU_1

Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.