This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 Ware与F28388D

Other Parts Discussed in Thread: TMDSCNCD28388D, C2000WARE

1、测试的设备:

TMDSCNCD28388D – HSEC180 controlCARD

2、测试的例程:

can_ex2_loopback_interrupts

3、例程所在的路径:

C:\ti\c2000\C2000Ware_3_03_00_00\driverlib\f2838x\examples\cm\can\CCS

4、测试的目的

初步的目的:

想要通过F28388D的CM核,跑CAN的程序

最终的目的:

    1、想要实现的功能是,STM32通过CAN发送数据,然后F28388D通过CANA中断接收。一条数据接受完毕后,返回一个接受完毕标志位。(这一句话的功能,要求 在CM核中实现)

     2、需要在CPU1中实现的功能是,检测到CM中的接收完成标志位,然后,将CM核中接收到数据的数组,传递到CPU1中,在CPU1核中完成数组数据的处理。处理完成之后,设置一个数据处理完毕标志位。此时,CM核查询到数据处理完毕标志位,通过CM核,控制串口,将处理后的数据发送给外界。

5、目前试着运行例程,存在的问题:

can_ex2_loopback_interrupts,这个例程,运行在CM后,应该是在变量的窗口,能看到txMsgData和rxMsgData的变化,但是,正如下图所示,只有txMsgData有变化。这个很奇怪。

6、关于F28388D的CPU1与CM核,如何实现这两个核之间的通信呢?

特来请教

谢谢!