This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在280049C上参考driverlib无法初始化LINA的问题

自己设计了1块280049C的板卡,主要实现SCI和LINA的功能,其中,LINA实现SCI的兼容功能。目前,已经实现了SCI模块的通信功能。但是在采用LINA的SCI兼容功能的时候,调用了LIN_initModule(LINA_BASE);,和configureSCIMode(void)两个函数,发现在LIN_initModule(LINA_BASE)代码里通过单步调试,发现在相对应的发送接收功能,波特率,字符长度等功能无法进行配置,同样的我采用了传统的寄存器直接配置方法,也无法实现,请问可能存在什么原因导致了这个问题?

  • 请向我们提供以下详细信息,以便我们为您提供更好的帮助。

    请问能否请您给出相关的代码?请确认您已经查看了TRM中的LIN配置部分: 27.3.5 LIN Configurations

    您现在硬件的话是几块板?均是自制板吗?是否使用loop模式?