This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS升级后之前版本的程序调试异常

Other Parts Discussed in Thread: C2000WARE

大家好,我想咨询一个问题:我最近把CCS从版本6升级到了版本10,但是发现升级后的CCS无法正常调试,每次运行都会弹出如下故障:

Break at address "0x3ff4fa" with no debug information available, or outside of program code.

测试的代码没有问题,仅仅是换了CCS的版本。不知道大家有没有遇到过同样的问题?

顺便问以下,CCS版本升级有什么用,本来版本6调用controlsuit的例程时说CCS版本低,要升级后才能调用,升级到CCS10后调用例程又显示没有XDAIS0.0,查询资料后说是新版本没有这个插件,还是用不了例程,网上说的方法都试了一遍都不行(在设置中关掉XDAIS或者重新下载调用),现在在新版本上运行之前好的程序又报上述错误,真的是无语。。。

  • user4369064 说:
    我最近把CCS从版本6升级到了版本10,但是发现升级后的CCS无法正常调试,每次运行都会弹出如下故障:

    之前在CCS6是可以正常调试的?若是可以的话,请私信您的工程,我们实际测试一下

    user4369064 说:
    CCS版本升级有什么用

    会有一些功能上的增强和更新,具体可以查看 ReleaseNotes,路径一般在 ccs1000\ccs\doc

  • “本来版本6调用controlsuit的例程时说CCS版本低,要升级后才能调用,升级到CCS10后调用例程又显示没有XDAIS0.0,查询资料后说是新版本没有这个插件,还是用不了例程,网上说的方法都试了一遍都不行(在设置中关掉XDAIS或者重新下载调用),”

    您可以直接使用C2000ware内的例程。若是您还是想使用controlsuit的例程,请给出您的例程路径,我们具体看一下