This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前DSP28335 需要在ADCA上采集8路ADC值,使用DMA搬运数据,代码如下
static void adc_config(void)
{
EALLOW;
SysCtrlRegs.HISPCP.all = ADC_MODCLK; // 150 / (2*3) = 20M
EDIS;
InitAdc();
AdcRegs.ADCTRL1.bit.ACQ_PS = ADC_SHCLK;
AdcRegs.ADCTRL3.bit.ADCCLKPS = ADC_CKPS;
AdcRegs.ADCTRL1.bit.SEQ_CASC = 1; // 0 Non-Cascaded Mode
AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 0x1;
AdcRegs.ADCTRL2.bit.RST_SEQ1 = 0x1;
AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; //选择管脚ADCINA0
AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1; //ADCINA1
AdcRegs.ADCCHSELSEQ1.bit.CONV02 = 0x2; //ADCINB0
AdcRegs.ADCCHSELSEQ1.bit.CONV03 = 0x3; //ADCINB1
AdcRegs.ADCCHSELSEQ2.bit.CONV04 = 0x4;
AdcRegs.ADCCHSELSEQ2.bit.CONV05 = 0x5;
AdcRegs.ADCCHSELSEQ2.bit.CONV06 = 0x6;
AdcRegs.ADCCHSELSEQ2.bit.CONV07 = 0x7;
AdcRegs.ADCMAXCONV.bit.MAX_CONV1 = 7; // Set up ADC to perform 4 conversions for every SOC
AdcRegs.ADCTRL1.bit.CONT_RUN = 1; //连续运行模式
AdcRegs.ADCTRL1.bit.SEQ_OVRD = 1; // Enable Sequencer override feature
}
static void adc_dmaconfig(void)
{
volatile unsigned int *dmadest;
volatile unsigned int *dmasource;
DMAInitialize();
memset((void *)dma_adcbuf, 0, sizeof(dma_adcbuf));
memset((void *)dma_adcbuf_end, 0, sizeof(dma_adcbuf_end));
dmadest = dma_adcbuf;
dmasource = &AdcMirror.ADCRESULT0; //Point DMA source to ADC result register base
DMACH1AddrConfig(dmadest, dmasource);
DMACH1BurstConfig(7, 1, 10);
DMACH1TransferConfig(9, 1, 0);
DMACH1WrapConfig(0, 0, 0, 1);
DMACH1ModeConfig(DMA_SEQ1INT, PERINT_ENABLE,
ONESHOT_DISABLE, CONT_DISABLE,
SYNC_DISABLE, SYNC_SRC,
OVRFLOW_DISABLE, SIXTEEN_BIT,
CHINT_END, CHINT_ENABLE);
StartDMACH1();
}
请问我是否可以控制ADC采集的是哪一路,也就是我现在需要第一路的数据时采集第一路,需要第二路的时候发一条指令采集第二路