在设计C2000芯片的PCB时,模拟地和数字地必须要接在一起,如果不接在一起,会存在压差。采用单点接地的方式,可以避免模拟地和数字地大面积相连造成的干扰。外部电源地或者您说的其他的方式连接存在很大的压差,相当于不是同一个地。
1、在电源部分,推荐的做法是AVCC与DVCC前独立加π型滤波;
2、在接地部分,需要注意不仅是单点接地,高速信号和模拟信号还需要有地平面的跟随,如果单点接地了但是数字信号跑到模拟地平面的区域了,这样也会造成很强的干扰,一方面在那一部分里面没有高速信号没有参考,另一方面会给模拟地平面造成高频干扰;
3、layout时候如果遇到布局走线不方便,可以使用半包围的方法进行,逐渐优化包围圈,使各类信号有自己的参考平面,地平面整齐,信号线整齐。