This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA00643电调母线电压问题

尊敬的TI你好:

我在使用贵公司所提供的TIDA00643时,遇到一些问题;

请问,TIDA00643在硬件上是否有限制母线电压?为什么我在使用CCS看母线电压测量值时,无论怎么改变电源电压值,所测得的母线电压值均为19.3V?

如果不是硬件限制,那能否通过软件进行修改?能够修改的话,在哪里修改呢?