Other Parts Discussed in Thread: LAUNCHXL-F28069M
对F28069进行调试时,直接点击Resume运行程序没有任何效果,需要先Restart一下,再运行才有效果;
之前对这个程序进行调试时没这个问题,可以直接进行调试;
而且如果将这程直接烧到Flash里,也没有反应,按了复位键也没反应,同样的之前也没有出现过这个问题
下面是主函数:
void main()
{
// Setup the system clock
// Disable the watch-dog timer, initialize the system clock,
// PLL and configure the peripheral clock.
InitSysCtrl();
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2806x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2806x_DefaultIsr.c.
// This function is found in F2806x_PieVect.c.
InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within my_PWM.c file.
EALLOW;
PieVectTable.EPWM1_INT = &epwm1_timer_isr;
EDIS;
// Initialize My ePWM Peripherals
InitMyEPwm();
// Enable CPU INT3 which is connected to EPWM1
IER |= M_INT3;
// Enable EPWM INTn in the PIE:GROUP3 interrupt 1
PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global real-time interrupt DBGM
// Copy time critical code and Flash setup code to RAM
// The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart
// symbols are created by the linker. Refer to the F2808.cmd file.
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32)&RamfuncsLoadSize);
// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
InitFlash();
// IDLE Loop.
while(1)
{
;
}
}