你好,
基于BOOSTXL-BUCKCONV(电源板)、TMS320F28379D(开发板)的数字电源程序。我已经实现了VMC的启动延迟和软起动功能,但是PCMC模式使用无法实现该功能,请问PCMC模式下可以实现软起动吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
基于BOOSTXL-BUCKCONV(电源板)、TMS320F28379D(开发板)的数字电源程序。我已经实现了VMC的启动延迟和软起动功能,但是PCMC模式使用无法实现该功能,请问PCMC模式下可以实现软起动吗?
非常感谢。
启动延时的实现简介,先判断输入电压是否达到启动电压,达到启动电压后,开启2ms定时器,定时器到了之后,设置输出参考电压。
软启动的实现,参照TMS320F280049C的示例代码没有做变更。
现在出现两种情况
1.延时启动添加后,输出电压几乎等于输入电压,PID算法无法调节
2.软起动也没有出现
3.按照TI的调试手顺,经常出现过电流检出现象
他的用途我们了解了,谢谢。还想问一下,我使用CMPSS控制EPWM。当Timebase等于0是,EPWMA置高,CMPSS比较输出为1时,EPWM拉低。
但是我们发现,CMPSS输出1时,EPWM并没有拉低。请问这可能是什么导致的?