我用的是 研旭的28335一体板,做整流的控制,simulink仿真是没有问题的,但是一到实验,只要用flash装载程序,一加电压,pwm输出波形就发生严重振荡,有大量高次谐波,连输入的交流电压也发生了畸变,产生了很多高次谐波,用仿真器的话,一加电压就会出现出错
”IcePick_C_0: Error: (Error -154 @ 0x0) One of the FTDI driver functions used to write data returned bad status or an error. (Emulation package 8.4.0.00006)
C28xx_CPU1: JTAG Communication Error: (Error -154 @ 0x0) One of the FTDI driver functions used to write data returned bad status or an error. (Emulation package 8.4.0.00006)
C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging“
我初步怀疑是不是功率电路对控制板产生的干扰,但是又无法确定,有没有遇到这类问题的朋友帮助解答一下呢