This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好。
DSP: LAUNCHXL-F280049C
数字电源控制板:BOOSTXL-BUCKCONV
Demo 代码:Resource Explorer TIDM-DC-DC-BUCK-DC-DC Synchronous Buck Converter
现象:
参照《TIDM-DC-DC-BUCK》,对应功能已经验证完成。
但是,当我打开CLA后,在PCMC模式下,输出电压波动较大(1.2v->1.5->1.8->1.5->1.2)。
CLA打开步骤:
1. buck_clatasks.cla加入编译
右击文件buck_clatasks.cla,将弹出菜单中的"Exclude from Build"的√去掉
2. 将BUCK_CONTROL_RUNNING_ON_CPU宏替换成BUCK_CONTROL_RUNNING_ON_CLA
3. 重新编译
问题:
1. CLA打开步骤是否存在问题?上述CLA打开步骤是否正确?
2. LAUNCHXL-F280049C+BOOSTXL-BUCKCONV+demo 应该怎么打开CLA?
3. 如果CLA打开步骤正确,请问是什么问题导致现在的现象?或者说有什么调查方向?