This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

lab21例程IPD_HFI如何控制电流大小?

Other Parts Discussed in Thread: DRV8301

使用的DRV8301kit_revD的实例lab21,开发套件是DRV8301-69M-KIT,

我使用的DC Power给开发板供电,电压设置为36V,电流设置为3.85;

目前的主要问题是l跑ab21例时,电源显示电流满载3.85A,电机很快发热;

正常情况下电流也都在0.5A以内,电机运行也很稳定;

为什么lab21时电流很不受限,直接满载?

我也有参考lab05加入gMotorVars.IqRef_A参数控制似乎也不能影响电流大小,或许是我做法不正常。

因为也是初次接触不具体应该何在lab21的基础上加入电流限制,望请赐教,谢谢!

电机参数:

额定电压:36V

额定电流:4.01A

额定转速:54900

程序参数配置如下:

#define USER_IQ_FULL_SCALE_FREQ_Hz (915.0) 

#define USER_IQ_FULL_SCALE_VOLTAGE_V      (36.0)

#define USER_ADC_FULL_SCALE_VOLTAGE_V       (66.32)      // 66.32 drv8301_revd voltage scaling

#define USER_PWM_FREQ_kHz                (60)

............................

#elif (USER_MOTOR == My_Motor)
#define USER_MOTOR_TYPE MOTOR_Type_Pm
#define USER_MOTOR_NUM_POLE_PAIRS (1)
#define USER_MOTOR_Rr (NULL)
#define USER_MOTOR_Rs (0.2044503)
#define USER_MOTOR_Ls_d (0.0003621753)
#define USER_MOTOR_Ls_q (0.0003621753)
#define USER_MOTOR_RATED_FLUX (0.0237821)
#define USER_MOTOR_MAGNETIZING_CURRENT (NULL)
#define USER_MOTOR_RES_EST_CURRENT (0.2)
#define USER_MOTOR_IND_EST_CURRENT (-0.2)
#define USER_MOTOR_MAX_CURRENT (4.01)
#define USER_MOTOR_FLUX_EST_FREQ_Hz (USER_IQ_FULL_SCALE_FREQ_Hz * 0.1)//约为额定转速10%

//下面HFI的参数部分用的默认参数,没有修改过

// IPD and AFSEL settings below are not necessarily valid for this motor
// Added so that proj_lab21 compiles without errors with default user.h settings
#define IPD_HFI_EXC_FREQ_HZ (750.0) // excitation frequency, Hz
#define IPD_HFI_LP_SPD_FILT_HZ (35.0) // lowpass filter cutoff frequency, Hz
#define IPD_HFI_HP_IQ_FILT_HZ (100.0) // highpass filter cutoff frequency, Hz
#define IPD_HFI_KSPD (60.0) // the speed gain value
#define IPD_HFI_EXC_MAG_COARSE_PU (0.25) // coarse IPD excitation magnitude, pu
#define IPD_HFI_EXC_MAG_FINE_PU (0.2) // fine IPD excitation magnitude, pu
#define IPD_HFI_EXC_TIME_COARSE_S (0.5) // coarse wait time, sec max 0.64
#define IPD_HFI_EXC_TIME_FINE_S (0.5) // fine wait time, sec max 0.4
#define AFSEL_FREQ_HIGH_PU (_IQ(20.0 / USER_IQ_FULL_SCALE_FREQ_Hz))
#define AFSEL_FREQ_LOW_PU (_IQ(10.0 / USER_IQ_FULL_SCALE_FREQ_Hz))
#define AFSEL_IQ_SLOPE_EST (_IQ((float)(1.0/0.1/USER_ISR_FREQ_Hz)))
#define AFSEL_IQ_SLOPE_HFI (_IQ((float)(1.0/10.0/USER_ISR_FREQ_Hz)))
#define AFSEL_IQ_SLOPE_THROTTLE_DWN (_IQ((float)(1.0/0.05/USER_ISR_FREQ_Hz)))
#define AFSEL_MAX_IQ_REF_EST (_IQ(0.4))
#define AFSEL_MAX_IQ_REF_HFI (_IQ(0.4))

  • 你是调试的IPD_HFI实验?IPD功能的调试相对自适应性会比FAST差一些,也就是根据不同电机需要调整的参数相对较多。
    但IPD工作的理论前提是电机需要有凸极效应,即Ld 与 Lq不相等,而且差距越大理论上IPD的估算效果越好,所以首先请先确定电机是否具有凸极效应,如果没有,那么算法是不能正常工作的。