This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2812中外部中断XINT13配置问题。

您好,我想使用XINT13这个外部中断,可是在使能PIE中断向量这一步时发现在PIE中断向量表中没有XINT13对应的中断,查阅数据手册时发现XINT13在INT13这里,请问这里的意思是XINT13这个外部中断不需要在PIE这一级使能,直接在CPU级使能就可以了吗?我需要如何配置才能正确使用XINT13这个外部中断呢?还有一个问题是XINT1\2\13这些外部中断在响应过后需要手动把中断标志位清除吗,如果需要的话,该向哪个寄存器里面写数据呢?谢谢。