使用官方的LauchPad TMS320F28027P开发板 加 Bootxstl DRV8305EVM 学习INSTASPIN-FOC,但是用CCS10编译 proj_lab05b,并且下载程序到LauchPad TMS320F28027P上,点击了时钟那个图标,并且点击运行,然后加载了proj_lab05b.js脚本文件, 在进行实时调试的时候无法进行。
C28xx: Trouble Writing Memory Block at 0xc0 on Page 1 of Length 0x1: (Error -1041 @ 0x800) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00042)
C28xx: Trouble Reading Register PC: (Error -1140 @ 0x0) Lost debug connection to device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.3.0.00042)
C28xx: Trouble Reading Register ST1: (Error -1156 @ 0x800) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.3.0.00042)
C28xx: 1 other operation(s) were automatically canceled as a result