This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035 ADC错位

Other Parts Discussed in Thread: TMS320F28035

Dear Teams,

我的客户在使用TMS320F28035的时候,写入的ADC通道和读取的不一样。具体信息参照以下:

下图是代码里把通道0和1配置为B1, 2和3配置为B2, 4和5配置为B6,6为A3, 7为A5等等。然后给不同通道不同电压,然后从寄存器的RESULT寄存器去读取数据,发现:最后发现从B1读取到的数据是1和2通道的,B2读到的是3和4通道的,B6读到的是5和6通道的,出现了往后移位。ADC寄存器的配置见附件。麻烦帮忙看下这会是什么原因导致的,或者有什么建议吗?谢谢adc.C

//----------------------------------------------------------------------------------
//	FILE:			ADC_SOC_CNF.c.c
//
//	Description:	ADC configuration to support up to 16 conversions on 
//					Start of Conversion(SOC) based ADCs (type 3) found on F2802x and 
// 					F3803x devices.  Independent selection of Channel, Trigger and 
// 					acquisition window using ChSel[],TrigSel[] and ACQPS[].
//
//  Dependencies:  Assumes the {DeviceName}-usDelay.asm is inlcuded in the project   
//	Version: 		2.0
//
//  Target:  		TMS320F2802x(PiccoloA), 
//					TMS320F2803x(PiccoloB), 
//
//  The function call is: 
//		
//		void ADC_SOC_CNF(int ChSel[], int Trigsel[], int ACQPS[], int IntChSel, int mode)
//
// Function arguments defined as:
//-------------------------------
// ChSel[]  = 	Channel selection made via a channel # array passed as an argument
// TrigSel[]= 	Source for triggering conversion of a channel, 
//			  	selection made via a trigger # array passed as argument
// ACQPS[]  = 	AcqWidth is the S/H aperture in #ADCCLKS,# array passed as argument
// IntChSel = 	Channel number that would trigger an ADC Interrupt 1 on completion(EOC)
//			    if no channel triggers ADC interrupt pass value > 15
// Mode 	= 	Operating mode: 	0 = Start / Stop mode, needs trigger event
//                             		1 = Continuous mode, no trigger needed
//									2 = CLA Mode, start stop mode with auto clr INT Flag
//================================================================================
#include "PeripheralHeaderIncludes.h"

void ADC_SOC_CNF(int ChSel[], int Trigsel[], int ACQPS[], int IntChSel, int mode)
{

	extern void DSP28x_usDelay(Uint32 Count);

 
	EALLOW;
	AdcRegs.ADCCTL1.bit.ADCREFSEL	= 0;
   	AdcRegs.ADCCTL1.bit.ADCBGPWD	= 1;	// Power up band gap
   	AdcRegs.ADCCTL1.bit.ADCREFPWD	= 1;	// Power up reference
   	AdcRegs.ADCCTL1.bit.ADCPWDN 	= 1;	// Power up rest of ADC
	AdcRegs.ADCCTL1.bit.ADCENABLE	= 1;	// Enable ADC

	DSP28x_usDelay(1000);         // Delay before converting ADC channels

	AdcRegs.ADCCTL1.bit.INTPULSEPOS	= 1;

	AdcRegs.ADCSOC0CTL.bit.ACQPS = ACQPS[0];
   	AdcRegs.ADCSOC1CTL.bit.ACQPS = ACQPS[1];
   	AdcRegs.ADCSOC2CTL.bit.ACQPS = ACQPS[2];
   	AdcRegs.ADCSOC3CTL.bit.ACQPS = ACQPS[3];
   	AdcRegs.ADCSOC4CTL.bit.ACQPS = ACQPS[4];
   	AdcRegs.ADCSOC5CTL.bit.ACQPS = ACQPS[5];
   	AdcRegs.ADCSOC6CTL.bit.ACQPS = ACQPS[6];
   	AdcRegs.ADCSOC7CTL.bit.ACQPS = ACQPS[7];
   	AdcRegs.ADCSOC8CTL.bit.ACQPS = ACQPS[8];
   	AdcRegs.ADCSOC9CTL.bit.ACQPS = ACQPS[9];
   	AdcRegs.ADCSOC10CTL.bit.ACQPS = ACQPS[10];
   	AdcRegs.ADCSOC11CTL.bit.ACQPS = ACQPS[11];
   	AdcRegs.ADCSOC12CTL.bit.ACQPS = ACQPS[12];
   	AdcRegs.ADCSOC13CTL.bit.ACQPS = ACQPS[13];
   	AdcRegs.ADCSOC14CTL.bit.ACQPS = ACQPS[14];
   	AdcRegs.ADCSOC15CTL.bit.ACQPS = ACQPS[15];

	AdcRegs.INTSEL1N2.bit.INT1SEL = IntChSel;		// IntChSel causes ADCInterrupt 1

	if (mode == 0)		// Start-Stop conv mode
	{
		AdcRegs.ADCINTFLG.bit.ADCINT1 = 0;  // clear interrupt flag for ADCINT1
		AdcRegs.INTSEL1N2.bit.INT1CONT = 0;	// clear ADCINT1 flag to begin a new set of conversions
	   	AdcRegs.ADCINTSOCSEL1.all=0x0000;	// No ADCInterrupt will trigger SOCx
	   	AdcRegs.ADCINTSOCSEL2.all=0x0000;
	}
	if (mode == 1)		// Continuous conv mode
	{
		AdcRegs.INTSEL1N2.bit.INT1CONT = 1;	// set ADCInterrupt 1 to auto clr
		AdcRegs.ADCINTSOCSEL1.all=0xFF;// ADCInterrupt 1 will trigger SOCx, TrigSel is ignored
		AdcRegs.ADCINTSOCSEL2.all=0xFF;
	}

	if (mode == 2)		// CLA mode, Start Stop ADC with auto clr ADC Flag
	{
		AdcRegs.ADCINTFLG.bit.ADCINT1 = 0;  // clear interrupt flag for ADCINT1
		AdcRegs.INTSEL1N2.bit.INT1CONT = 1;	// set ADCInterrupt 1 to auto clr
		AdcRegs.ADCINTSOCSEL1.all=0x0000;	// No ADCInterrupt will trigger SOCx
	   	AdcRegs.ADCINTSOCSEL2.all=0x0000;
	}

	if(IntChSel<15)
		AdcRegs.INTSEL1N2.bit.INT1E = 1;		// enable ADC interrupt 1
	else
		AdcRegs.INTSEL1N2.bit.INT1E = 0;		// disable the ADC interrupt 1

// Select the channel to be converted when SOCx is received
	AdcRegs.ADCSOC0CTL.bit.CHSEL= ChSel[0];
	AdcRegs.ADCSOC1CTL.bit.CHSEL= ChSel[1];
	AdcRegs.ADCSOC2CTL.bit.CHSEL= ChSel[2];
	AdcRegs.ADCSOC3CTL.bit.CHSEL= ChSel[3];
	AdcRegs.ADCSOC4CTL.bit.CHSEL= ChSel[4];
	AdcRegs.ADCSOC5CTL.bit.CHSEL= ChSel[5];
	AdcRegs.ADCSOC6CTL.bit.CHSEL= ChSel[6];
	AdcRegs.ADCSOC7CTL.bit.CHSEL= ChSel[7];
	AdcRegs.ADCSOC8CTL.bit.CHSEL= ChSel[8];
	AdcRegs.ADCSOC9CTL.bit.CHSEL= ChSel[9];
	AdcRegs.ADCSOC10CTL.bit.CHSEL= ChSel[10];
	AdcRegs.ADCSOC11CTL.bit.CHSEL= ChSel[11];
	AdcRegs.ADCSOC12CTL.bit.CHSEL= ChSel[12];
	AdcRegs.ADCSOC13CTL.bit.CHSEL= ChSel[13];
	AdcRegs.ADCSOC14CTL.bit.CHSEL= ChSel[14];
	AdcRegs.ADCSOC15CTL.bit.CHSEL= ChSel[15];


	AdcRegs.ADCSOC0CTL.bit.TRIGSEL= Trigsel[0];
	AdcRegs.ADCSOC1CTL.bit.TRIGSEL= Trigsel[1];
	AdcRegs.ADCSOC2CTL.bit.TRIGSEL= Trigsel[2];
	AdcRegs.ADCSOC3CTL.bit.TRIGSEL= Trigsel[3];
	AdcRegs.ADCSOC4CTL.bit.TRIGSEL= Trigsel[4];
	AdcRegs.ADCSOC5CTL.bit.TRIGSEL= Trigsel[5];
	AdcRegs.ADCSOC6CTL.bit.TRIGSEL= Trigsel[6];
	AdcRegs.ADCSOC7CTL.bit.TRIGSEL= Trigsel[7];
	AdcRegs.ADCSOC8CTL.bit.TRIGSEL= Trigsel[8];
	AdcRegs.ADCSOC9CTL.bit.TRIGSEL= Trigsel[9];
	AdcRegs.ADCSOC10CTL.bit.TRIGSEL= Trigsel[10];
	AdcRegs.ADCSOC11CTL.bit.TRIGSEL= Trigsel[11];
	AdcRegs.ADCSOC12CTL.bit.TRIGSEL= Trigsel[12];
	AdcRegs.ADCSOC13CTL.bit.TRIGSEL= Trigsel[13];
	AdcRegs.ADCSOC14CTL.bit.TRIGSEL= Trigsel[14];
	AdcRegs.ADCSOC15CTL.bit.TRIGSEL= Trigsel[15];
	EDIS;

	AdcRegs.ADCSOCFRC1.all = 0xFFFF;		// kick-start ADC

}