This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
[2021/5/10 下午5:59:06] [INFO] C28xx_CPU1: GEL Output: Memory Map Initialization Complete
[2021/5/10 下午5:59:10] [ERROR] C28xx_CPU1: Error: (Error -1044 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00042)
[2021/5/10 下午5:59:10] [ERROR] C28xx_CPU1: Trouble Halting Target CPU: (Error -1135 @ 0xC095) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00042)
[2021/5/10 下午5:59:11] [ERROR] C28xx_CPU1: Unable to determine target status after 20 attempts
[2021/5/10 下午5:59:11] [ERROR] C28xx_CPU1: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x00130@Program: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error executing PLL configuration algorithm. Operation cancelled. (0x0)
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: File Loader: Memory write failed: Unknown error
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read register PC: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005F800@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005FC00@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_en.alg
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D22E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D208@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D208@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D222@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D214@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D20E@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x0005D222@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000@Program: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Cannot enable while the target is disconnected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not read 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Failed to run target while trying to execute pwrite_dis.alg
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash. If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG) register and the Boot-ROM status register for further debug.
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write 0x00000064@Data: target is not connected
[2021/5/10 下午5:59:31] [ERROR] C28xx_CPU1: Error occurred during flash operation: Could not write register PC: target is not connected
根据您的描述,看起来是这两块板子本身的硬件连接问题
您可以看一下该链接内给出的相关帖子
This error is commonly associated with C28x devices and is usually associated with a range of hardware or firmware problems that prevent the JTAG debugger to connect to the core.