This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28069内部电源问题

Other Parts Discussed in Thread: CONTROLSUITE

自己做的28069的板子,和controlsuite里的28069开发板基本相同,Vdd1.8 采用的是内部供电,连接一个2.2uF电容接地,上电后,3.3V正常,1.8V没有,导致芯片无法正常工作,请问是什么原因,会是芯片坏了吗?

  • 确定Pin90 VREGENZ是拉低的吗?建议量量信号检查一下先。

  • 确实已经拉低,3.3V稳定,内部1.8V就不正常了,请问有可能是芯片的原因吗

  • 它应该是低电平,才可能有正常的1.8V输出,所以看起来不是这个引脚的问题。

    请重新确定一下电源的波形,以及看看其电流多大?是否可以尝试使用外部直流源,限流至0.2或0.5A看一下?

    同时可以看看复位信号是否正常?有没可能连接或焊接有问题--整个芯片,以及电源引脚等?

    另外,如果仍有问题,或许你可以将原理图发出来检查下。

    最后,你也可以尝试换一块板子或一颗芯片试试,不能确定是否被损坏了的话。