Part Number: TMS320F28035
您好,请问一下,CLA的CLARAM0和 CLARAM1的区域必须固定为RAML1和RAML2区域吗?Cla1Prog固定为RAML3?由于C28中变量过多,原有的RAM区域不够需要扩展,需要修改cmd中的RAM区域,目前占用了RAML1区域,把CLARAM0改为RAMM1所在区域可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
您好,请问一下,CLA的CLARAM0和 CLARAM1的区域必须固定为RAML1和RAML2区域吗?Cla1Prog固定为RAML3?由于C28中变量过多,原有的RAM区域不够需要扩展,需要修改cmd中的RAM区域,目前占用了RAML1区域,把CLARAM0改为RAMM1所在区域可以吗?
您好,感谢您的回复,我的意思是地址,使能CLARAM0的地址是固定的吗?
Cla1Regs.MMEMCFG.bit.PROGE = 1;
Cla1Regs.MCTL.bit.IACKE = 1;
Cla1Regs.MMEMCFG.bit.RAM0E = CLARAM0_ENABLE;
CLARAM0和CLARAM1可以在RAML0、RAML1和RAML2,Cla1Prog固定为RAML3。L3是F2803x上唯一可用于程序存储器的RAM块。