您好,制作了5块F28M35的板子,3块可以正常工作,其中两个出现了一些问题。如下:
1、上电启动后,复位引脚XRS上电后持续低电平,导致无法连接仿真器。
2、上电启动后,测试3.3V、1.2V和1.8V内核电压,其中3.3V和1.2V正常,1.8V处输出2.4V,有问题(手册上显示1.8供ANOLOG子系统)。
3、时钟外供30M,测试正常。
紧急因对:强制将复位信号拉高,M3核可以正常工作,但是C28核仿真器始终连接不上,报错如下:
C28xx_0: Error connecting to the target: (Error -1155 @ 0x0) Device may be operating in low-power mode. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0)
咨询TI专家,这种情况是否是芯片损坏了,导致一些功能不正常。电源设计是参考官方手册设计,还请看下下图电源是否有问题?
电源及复位电路如图: