This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
使用F28M35设计电路的时候,忽略了BOOT引脚的设计,将PF2/PF3/PG3/PG7用于了外设。
现在想让程序从FLASH中启动,查看手册,需要将PF3/PG3/PG7引脚上电初始化时保持高电平。我在当前设计基础上(PF2/PF3/PG3/PG7连接外设,均为输出类型),直接加上拉电阻,是否能满足MODE5从FLASH启动?同时加的上拉电阻是否影响原来外设的工作?多少的上拉电阻合适?
谢谢!