This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: TMS320F28069 和28035中adc采样区别

Part Number: TMS320F28069


1.DSP28069和DS928035中ADC在配置中有啥特别的区别吗?

2.我现在遇到一个问题,用28035主频60MHz采样的电压信号,很精确,

3.但是用了90M的28069后,电压采样不够线性,也不够精确,

4、将28069的系统主频我配置成60m后,和3同样的adc配置,电压采样信号,精度很好,和28035很一致。

第3和第4种情况,同样的是28069,只是主频不一样,但是采样结构却完全不一样。这是什么原因造成的?采样我也放在pwm中断中进行的,pwm中断频率都是一样的100khz。