This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我在连接仿真器时,出现了如下问题,请问怎么解决?我测试的硬件没有问题。
[Start: Texas Instruments XDS100v2 USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\Lenovo\AppData\Local\TEXASI~1\CCS\
ccs9.3\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.
The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
[End: Texas Instruments XDS100v2 USB Debug Probe_0]
[Start: UARTConnection_0]
Execute the command:
The Diagnostic Command is not defined in the connection properties.
您可以看一下
给出的相关信息。请问您现在使用的是TI开发板?能否给出型号?
您好,我仿照的是launchxl_F28379d这个板子自己画的板子
唯一的区别是这是launchxl_F28379d的原理图
我画的是;
请问这些会有有影响吗?
仿真器部分已解决
我将EEPROM换成原装的器件,就可以烧录进去程序了。应该是我买的器件型号不匹配。
请问,我板子之前通电一切正常,结果正在运行程序过程中,突然28379芯片烧坏,拆下来测试发现3.3v ,1.2V与GND之间短路,这种现象是怎么情况?
我板子之前通电一切正常,结果正在运行程序过程中,突然28379芯片烧坏,拆下来测试发现3.3v ,1.2V与GND之间短路,这种现象是怎么情况?
抱歉,之前请假未能及时回复。请问您现在问题解决了吗?