This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D-EP: TIDM-HV-1PH-DCAC例程采样方式切换

Part Number: TMS320F28377D-EP
Other Parts Discussed in Thread: TIDM-HV-1PH-DCAC, SYSCONFIG, POWERSUITE, C2000WARE

TIDM-HV-1PH-DCAC例程使用SDFM-based采样方式,但我需要使用ADC采样方式,我需要做哪儿些更改呢?

在Build-Level1-Open Loop模式下,我尝试做了些更改,但是查看采样结果寄存器数值为0。已做的更改有:

1、屏蔽main.syscfg,将sysconfig生成的gridconnectedinvlclfltr_settings.h文档迁移至工程目录下;

2、将gridconnectedinvlclfltr_settings.h文档中的SENSING_OPTION切换为2,用于切换至ADC采样;

  • 看起来您是在并网模式下运行。

    建议您参考这个帖子:

    https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/813597/ccs-tidm-hv-1ph-dcac-adc-sensing-method 

  • 对方回复:if you are doing something custom you can always import the project without powerSUITE and change according to you board and design.

    这个要怎么操作呢?

  • 抱歉,我们不支持电网连接代码上的 ADC 感应,因为电路板使用 SDFM 作为电网输出电流。

    如果您想在没有powerSUITE的情况下导入项目,可以直接从这里导入

    C:\ti\c2000\C2000Ware_DigitalPower_SDK_3_02_00_00\solutions\tidm_hv_1ph_dcac\f28004x\ccs\gridconnectedinvlclfltr

    这将在没有 powerSUITE 的情况下导入项目,可以自由修改项目以进行开发。